• Operation and Maintenance
  1. Home
  2. Wind Power Solutions

Advanced manufacturing and integrated O&M excellence for wind turbines

WEG combines advanced manufacturing technology and operational expertise to set the industry benchmark for performance and reliability.

Our dedicated team of skilled engineers and technicians delivers a full suite of services - from commissioning and start-up to operation, maintenance, and specialized repairs - ensuring your turbines operate with maximum availability and efficiency.

Backed by a strong presence in the United States, WEG provides technical depth, flexibility and dependable support to safeguard your assets’ efficiency and operational lifespan.

Partner with WEG to maintain peak performance, extend turbine lifetime, and deliver lasting value across your wind energy operations.

Operation

WEG performs round-the-clock (24/7) fleet monitoring through a dedicated digital platform, enabling effective asset management and real-time asset oversight to ensure equipment reliability.

Our advanced platform integrates machine learning and artificial intelligence for early anomaly detection, predictive diagnostics and automated workflows for seamless execution. Ongoing upgrades and robust data-driven insights drive continuous improvement, ensuring that all defined Key Performance Indicators are consistently met or exceeded.

That’s how WEG safeguards superior turbine availability and consistent performance.

Maintenance

WEG designs customized annual preventive maintenance schedules in close collaboration with each customer to minimize impacts on energy production.

By leveraging artificial intelligence and advanced analytics, we proactively identify and address maintenance needs, enabling early diagnostics and timely corrective actions that maximize turbine uptime and prevent energy production losses.

Our service capabilities range from routine preventive maintenance to complex corrective repairs, supported by custom tools, tailored proprietary procedures, and strong collaboration with local partners for agile and high-quality service.

Centro de Operação, Manutenção e Distribuição

Além da nossa matriz, localizada em Jaraguá do Sul/SC, a WEG conta com uma Filial WEG na cidade de Aracati/CE, onde prestamos suporte e fornecimento de peças para projetos localizados em todo Brasil, de forma ágil e estratégica.

O Centro de Operação, Manutenção e Distribuição possui estoque de peças das diferentes plataformas de Aerogeradores WEG para suporte aos parques da região Nordeste, além de dispositivos especiais para grandes corretivas e equipe local para gestão dos materiais e dispositivos/ferramentas.

Scope

WEG provides specialized technical services for the operation and maintenance of wind turbines and SCADA system.

Our O&M Services are available in two core packages, summarized below.

WEG also offers the flexibility to customize service scopes, ensuring alignment with each customer’s unique operational goals, requirements and preferences.

Stay updated with WEG's news in Wind Energy

Innovative partnership between WEG, Petrobras, and Statkraft brings the largest onshore wind turbine in the Americas into operation

Innovative partnership between WEG, Petrobras, and Statkraft brings the largest onshore wind turbine in the Americas into operation

Modernization project of the Brotas de Macaúbas Complex will increase efficiency and reinforce the pioneering spirit of the venture with a 7MW installed capacity turbine

WEG and Statkraft Sign Partnership for Implementation of the Largest Onshore Wind Turbine Produced in Brazil

WEG and Statkraft Sign Partnership for Implementation of the Largest Onshore Wind Turbine Produced in Brazil

The partnership will promote the installation of a wind turbine in the Brotas de Macaúbas Wind Complex in Bahia

WEG and Petrobras sign a partnership agreement for the development of the largest wind turbine in the country

WEG and Petrobras sign a partnership agreement for the development of the largest wind turbine in the country

The equipment will have a capacity of 7 MW and will be the first of its kind in Brazil

WEG confirma participação no maior evento de energia eólica da América Latina

WEG confirma participação no maior evento de energia eólica da América Latina

A feira Brazil Windpower acontece de 12 a 14 setembro no São Paulo Expo

WEG supplies motors to a platform to test and validate wind turbine technology

WEG supplies motors to a platform to test and validate wind turbine technology

Equipment will be part of the largest and most powerful powertrain and gearbox test bench in the world

WEG announces agreement with 2W Ecobank for self-production of wind power

WEG announces agreement with 2W Ecobank for self-production of wind power

The initiative will guarantee the supply of renewable energy in five industrial facilities of the Company in Brazil

WEG and Alupar sign agreement for self-production of wind power

WEG and Alupar sign agreement for self-production of wind power

Project will reinforce the energy supply of four industrial plants and the Company's commitment to sustainability

WEG Transformers and Shunt Reactors are supplied for a wind farm in northern Colombia

WEG Transformers and Shunt Reactors are supplied for a wind farm in northern Colombia

The equipment is part of a wind farm project with 492MW power capacity

WEG to launch a 7 MW wind turbine

WEG to launch a 7 MW wind turbine

The prototype should be ready for operation by 2024 and regular production to start in 2025

WEG supplies product package for a solar and wind power plant in Brazil

WEG supplies product package for a solar and wind power plant in Brazil

Five solar and wind power projects will be benefited by this product supply.

WEG and Engie Brasil Energia complete installation of the first national wind turbine

WEG and Engie Brasil Energia complete installation of the first national wind turbine

Wind turbine is part of the project for the first National Wind Turbine, which is intended to develop national technology and production chain for the manufacture and installation of large size equipment in the country

WEG joins a Business Mission to India

WEG joins a Business Mission to India

The "India - Brazil Business Forum”, was organized by the Brazilian Export and Investment Promotion Agency (Apex-Brasil) and took place in New Delhi, India.

WEG signs an agreement to supply wind turbines to Aliança Energia´s Wind Farms

WEG signs an agreement to supply wind turbines to Aliança Energia´s Wind Farms

The entire agreement includes the construction of four wind farms, in a total amount of 180.6 megawatts (MW) of installed capacity

WEG anuncia la entrada en el mercado eólico Hindú

La compañía tiene la intención de ajustar su fábrica de motores y generadores, en el estado de Tamil Nadu, cerca de Bangalore, para tambi...

WEG suministra paquete eléctrico completo para un complejo de energía eólica

Nuevo complejo eólico generará 230 MVA, potencia suficiente para abastecer a 400.000 hogares, lo que equivale a una ciudad con más de un ...

WEG Auxilia en la Generación de Energía Hidroeléctrica para Windsor Castle

La Eficiencia es el objetivo clave para esta aplicación, así como el hecho de que la instalación tenga un período de retorno de inversión...

WEG establishes a Joint Venture to produce wind turbines

WEG and the Spanish company - M. Torres Olvega Industrial (MTOI) – have established a Joint Venture for the manufacturing of wind turbine...

WEG MEXICO, S.A. DE C.V
  • Carretera Jorobas - Tula Km 3.5, Manzana 5, Lote 1, Fraccionamiento Parque Industrial Huehuetoca, Municipio de Huehuetoca - 54680 - CD. de México y Área Metropolitana / Mexico
  • Phone: +52 55 5321 4275 (Ventas Nacionales) / +52 55 5321 4210 (Ventas Internacionales)
  • Email: info-mx@weg.net
  • para centroamerica contacte: rfq-wmx@weg.net