WEG
  • Index
  • Products
    • SUSTAINABLE PRODUCTS AND SOLUTIONS
    • Technologies and Innovation for Energy Transition and Decarbonization
    • Responsible supply chain
  • Operations
    • CIRCULAR AND EFFICIENT OPERATIONS
    • Eco-efficiency and Waste and Emission Management
    • Carbon Neutral in Operations
  • People
    • ENGAGED EMPLOYEES AND COMMUNITIES
    • Sustainable Growth of the Communities
    • Comprehensive Well-being, Diversity and Inclusion
  • Governance
    • GOVERNANCE AND ETHICAL CONDUCT
    • Engagement and Transparent Communication
    • Compliance and Integrity
WEG - Driving efficiency and sustainability

Eco-efficiency and Waste and Emission Management

Circular and efficient operations

The circular economy seeks to maximize the value of resources while minimizing waste and environmental impacts. In this model, products are designed to be durable, repairable and recyclable, encouraging the reuse and recycling of materials. Instead of following the traditional linear model of production and consumption, in which products are manufactured, used and discarded, the circular economy promotes the idea of a continuous cycle, where materials are kept in use for as long as possible.

This approach not only contributes to the conservation of natural resources but also stimulates innovation, job creation and sustainable economic growth, making it essential to address today's global challenges such as climate change and resource scarcity.

Consolidating WEG's commitment, we have ISO 14,001 certifications demonstrating environmental management in the company's operations.

Programs & Practices

Residues and energy

Solid residues

WEG operations have a selective waste collection system. In this way, residues are separated and sent to recyclers of each material, enabling their appreciation and the reintroduction of such materials in different production cycles. It is important to emphasize that part of the waste generated in the operations is recycled by WEG itself, returning to the process and forming part of its products. All waste is sent to environmentally responsible companies, selected and developed by WEG's environmental management team.

See more

 

Energy

WEG has had an Energy Efficiency Policy since 2012, showing its commitment to the management of this input. This policy is deployed into actions to monitor and reduce energy consumption, which contributes to improving the environment. WEG intends to increasingly make its energy sources cleaner, renewable and sustainable.

Water, effluents and water resources

WEG monitors the water consumption of its operations and has several operational controls that ensure efficient management of this resource, thus avoiding waste and promoting conscious consumption. All effluents generated in operations are properly treated and periodically monitored in order to ensure compliance with legislation and minimize impacts on different stakeholders.

 

Part of the effluents treated in the operations are reused in the internal processes, where some effluent treatment plants enable the reuse of up to 100% of the treated effluent. We have adopted initiatives focused on reducing water consumption and effluent generation by controlling leaks, monitoring consumption and counting on the support of programs that engage all employees in this objective, such as KaizenWEG and WEG Manufacturing System.

 

Investments and expenses in the environment

Environmental investments fall into three categories:

  • Environmental control: related to treatment and disposal of residues, treatment of atmospheric and liquid emissions, environmental liability insurances, depreciation of devices and expenses with materials and maintenance.
  • Equipment: related to the purchase of equipment for environmental control.
  • Management: related to the remuneration of training staff who act in environmental management, research and development, and certification of environmental management systems.

Sustainable packaging and biodiversity preservation

We have a packaging factory, RF Reflorestadora, in Brazil. This unit produces all the wooden packaging used in our various product lines. To that end, we have our own reforestation areas that guarantee the continuous supply of wood and the preservation of this natural resource and areas of natural forests, legal reserves and permanent preservation areas that help in the preservation of the local biodiversity.

The areas comply with all legislation and legal requirements, including an area of conservation of native forests much larger than the minimum established for the legal reserve.

Furthermore, WEG promotes and supports conscious reforestation and nature conservation initiatives and invests in the afforestation of its industrial parks.

KaizenWEG

KaizenWEG fue creado en 2016 y es el corazón del sistema de gestión de mejora continua de WEG, el WMS, donde todos los colaboradores son incentivados a promover mejoras en su entorno de trabajo o en cualquier otra área de la empresa, identificando desperdicios, analizando causas y participando en equipos multidisciplinarios para la resolución de problemas. 

Siendo uno de los pilares de la Gestión Participativa de la Compañía, desde su creación se han implementado más de 300 mil mejoras, aportando mayor seguridad, calidad y productividad, además de hacer el entorno laboral cada vez más eficiente y sostenible.

La búsqueda colectiva de la excelencia operativa y la sostenibilidad en un escenario de verticalización de procesos convierte a la gestión participativa en una pieza clave para potenciar los resultados de WEG.

Mira el video del lanzamiento de la nueva plataforma de KaizenWEG: 

Video de lanzamiento

 

WMS (WEG Management System)

El sistema de gestión de mejora continua de WEG es el WMS, que tiene como principal objetivo la identificación y eliminación de pérdidas y desperdicios.

Los resultados son maximizados a través de las matrices de priorización de seguridad, calidad, costo y emisiones de GEE (gases de efecto invernadero horno), que direccionan la implementación de proyectos de optimización o eliminación de estos desperdicios, contribuyendo a un mundo más eficiente y sustentable.

Además de los frentes de trabajo de optimización, equipos multidisciplinarios actúan como puntos focales de mejora continua, trayendo innovaciones y disrupciones a nuestros procesos.

Uno de estos puntos de foco es el pilar de Medio Ambiente y Energía, que focaliza y sistematiza la reducción de impactos ambientales, actuando para reducir o eliminar la generación de residuos y emisiones, el consumo de recursos energéticos, limpiezas químicas e insumos en general.

Conozca más

 

Plan de Intercambio WEG (Disponible solo en Brasil)

El reciclaje es un tema serio para WEG, extendiéndose incluso a su negocio. Mediante el programa de reutilización de motores eléctricos, el "Plan de Intercambio", la empresa otorga un descuento en la compra de un nuevo motor con un rendimiento superior a los requisitos legales a cambio de uno usado. Además del beneficio financiero para los clientes, la iniciativa garantiza que el motor de baja eficiencia ya no se utilice. Una vez recogidos por la empresa, los motores se desmantelan y se separan en piezas para ser distribuidos a recicladores acreditados y rastreados.

 

Beneficios

  • Reducción del consumo de energía eléctrica

  • Confiabilidad de la planta

  • Reducción de costos operativos

  • Garantía de fábrica

  • Productos normalizados: ofrecen total intercambiabilidad con motores ya instalados

 

Item

2021

2022

2023

2024

Productos vendidos que pueden ser reutilizados o reciclados* (%) - Base en peso

68

73

65

70

Productos que fueron realmente reaprovechados o reciclados por la empresa* (%) - Base en peso

12

16

14

4

 

*Porcentaje basado en el peso de los productos vendidos en el año.

 

Inversiones en Medio Ambiente

Las inversiones ambientales se clasifican en dos categorías:

Inversiones de capital: Se refieren a la adquisición de equipos de control ambiental.

Gastos operativos (R$): Se refieren al tratamiento y disposición de residuos, el tratamiento de emisiones atmosféricas y líquidas, el seguro de responsabilidad ambiental y la depreciación de equipos, así como a los gastos de materiales y mantenimiento, y a los gastos de remuneración del personal que trabaja en gestión ambiental, investigación y desarrollo, y certificación de sistemas de gestión ambiental.

A continuación, se detalla el monto invertido en cada categoría:

 

Item

2021

2022

2023

2024

Inversión de capital (R$)

1.329.000

1.788.000

1.819.000

11.141.393

Gastos operativos (R$)

14.684.000

17.753.000

23.509.000

33.605.910

% de cobertura (%) 70 70 70 89

 

 

Certificación Ambiental

En 2024, considerando el alcance de los empleados, el 70,8% del grupo WEG estaba cubierto por la certificación ISO 14001.

Haga clic aquí para acceder a los certificados

 

Auditorías ambientales

WEG cuenta con un proceso de auditoría ambiental que abarca todas sus operaciones industriales.

En el proceso de auditoría ambiental anual, WEG garantiza el cumplimiento de la legislación ambiental en todas sus operaciones industriales.

 

Indicadores de Rendimiento

En 2023, se amplió el alcance de las unidades monitorizadas, incluyendo las direcciones comerciales de la empresa. Así, ahora el 100 % de las direcciones globales de WEG están incluidas en los indicadores.

Energía

WEG tiene una política de eficiencia energética desde 2012, en la que muestra su compromiso con la gestión de este recurso. Esta política desarrolla acciones para monitorear y reducir el consumo de energía, lo que contribuye a mejorar el medio ambiente. WEG tiene la intención de hacer cada vez más limpias, renovables y sostenibles sus fuentes de energía.

Consumo Total de Energía

Unidad

2019

2020

2021

2022

2023

Consumo total de energía no renovable

MWh

466,737 462,976 499,355

478,872

430,848

Consumo total de energía renovable

MWh 0

0

56,000

86,918

127,709

Consumo total de energía (no renovable + renovable)

MWh 466,737

462,976

555,355

565,790 558,557

Cobertura de datos (% del denominador)

porcentaje de empleados

100 100 100 100 100

Adquisición de energía renovable

En 2023, WEG garantizó que el 22,9% del consumo de energía procediera de fuentes renovables con garantía de origen mediante autoproducción, compra de certificados de energía renovable (I-REC) y contratos bilaterales.

En 2024, WEG tendrá aproximadamente el 90% del consumo de electricidad de Brasil proveniente de fuentes renovables, lo que equivale a un promedio de 45 MW.

 

Emisiones atmosféricas

WEG monitorea las emisiones atmosféricas relacionadas con compuestos orgánicos volátiles. A continuación se muestra el resultado de las emisiones relacionadas con equipos monitoreados en los últimos años.

 

Item

2019

2020

2021

2022

2023

2024

Emisiones de compuestos orgánicos volátiles (COV) (toneladas/año)

93,5 135,2 114,5

139,3

191,3 241,3

Tasa de cobertura (%)

56

56

56

61

72

61

Infracciones ambientales

Una de las principales prioridades de WEG es cumplir con la legislación ambiental aplicable a sus operaciones. En los últimos 4 años, no hubo evidencia de multas ambientales significativas aplicadas a las actividades de WEG.

Saiba mais sobre as ações da WEG em Sustentabilidade

WEG Tintas na Argentina adota energia 100% renovável em parceria com a 360Energy

WEG Tintas na Argentina adota energia 100% renovável em parceria com a 360Energy

Projeto reforça o compromisso da WEG com a descarbonização da indústria e o uso de fontes de energia limpas.

WEG oferece soluções de acabamento técnico para ambientes de saúde

WEG oferece soluções de acabamento técnico para ambientes de saúde

Tecnologia em revestimentos em pó combina proteção, segurança operacional e sustentabilidade em aplicações hospitalares

WEG apresenta Relatório Anual Integrado 2025 e destaca avanços em sustentabilidade

WEG apresenta Relatório Anual Integrado 2025 e destaca avanços em sustentabilidade

Resultados refletem investimentos em inovação, desenvolvimento de pessoas e avanços consistentes em ações ESG

WEG apoia a preservação de patrimônio industrial do Reino Unido com solução Motion Drives

WEG apoia a preservação de patrimônio industrial do Reino Unido com solução Motion Drives

Projeto desenvolvido com a Sheffield Transmission permite a operação segura e sustentável de uma máquina a vapor histórica de 1855 sem modificações estruturais

Eficiência energética e automação: Móveis Videira moderniza filtro de mangas com solução WEG

Eficiência energética e automação: Móveis Videira moderniza filtro de mangas com solução WEG

Setor moveleiro avança em sustentabilidade com economia média de 32% no consumo de energia

Grupo WEG
  • Avenida Prefeito Waldemar Grubba, 3300 - 89256-900 - Jaraguá do Sul - SC
  • Telefone: +55 47 3276 4000
  • E-mail: esg@weg.net






 

Instagram LinkedIn YouTube

 



 
WEG - Driving Efficiency and Sustainability