WEG
  • Index
  • Products
    • SUSTAINABLE PRODUCTS AND SOLUTIONS
    • Technologies and Innovation for Energy Transition and Decarbonization
    • Responsible supply chain
  • Operations
    • CIRCULAR AND EFFICIENT OPERATIONS
    • Eco-efficiency and Waste and Emission Management
    • Carbon Neutral in Operations
  • People
    • ENGAGED EMPLOYEES AND COMMUNITIES
    • Sustainable Growth of the Communities
    • Comprehensive Well-being, Diversity and Inclusion
  • Governance
    • GOVERNANCE AND ETHICAL CONDUCT
    • Engagement and Transparent Communication
    • Compliance and Integrity
WEG - Driving efficiency and sustainability
 

Technologies and Innovations for Energy Transition and Decarbonization

 

Through the company’s strategic direction towards its business model, WEG offers in all its business units more efficient solutions and products with lower environmental impact, such as renewable energy (solar, wind), electric mobility, energy efficiency, among others. WEG develops products considering strict risk criteria related to health and safety. During the development phase, analyses are applied, such as: Quality Function Deployment (QFD) and Risk Assessment.

Quality Management System

WEG applies a certified quality management system, based on external requirements and the requirements of our customers.

See more

Below are some highlights considering the variety of products and solutions the company provides to the market through its different business units.

Energy and Industrial Efficiency

W51 HD Motor (High Density)

Efficient and compact solution thar delivers high performance with reduced size and weight in comparison to the previous line (up to 25% higher power density – kW/kg) and its competitors. Therefore, it makes rational use of raw materials in the manufacture of motors and reduces the potential effects of their transformation, cutting down GHG emissions by about 15% in comparison to the previous line.

VSD for Motors

High-tech VSD for driving and controlling three-phase induction and permanent magnet motors. Thanks to its technology, this VSD model provides energy savings, safety, increased productivity and quality in the process network in which it is implemented. The CFW900, together with permanent magnet motors, offers the highest energy efficiency solution on the market. The new HMI with Bluetooth® connectivity is ideal for panel builders and repair shops, enabling programming, monitoring, parameter backup and other functionalities via tablets or smartphones.

BLDC Motor Line (Brushless DC)

For application in front load washing machines, it delivers a 60% improvement in the performance of the operating cycle and, consequently, a reduction of GHG emissions during the operation phase. This line currently represents 20% of the volume sold by WEG for front load washing machines.

Renewable Energy

Wind Power

In July 2022, WEG announced the release of a new wind turbine platform with 7 MW power and 172 meters of blade rotor diameter. This wind turbine will become the largest machine in operation in the Brazilian market. More powerful and efficient, the new model brings greater generation to wind projects.

Solar Power

WEG established itself as one of the main suppliers of products and solutions for solar plants in Brazil, bringing efficiency that drives sustainability in cities, industries, agribusiness and homes across the country. WEG has a vast portfolio of products for all the stages of photovoltaic solar generation projects, with solutions for the energy conversion and internal distribution system, from the plant to the point of connection to the electrical system through high voltage substations.

Hydroelectric Generation

WEG was selected to supply the generators for São Roque Hydroelectric Power Plant, located in the city of Vargem-SC. The generators are one of the most important parts of the enterprise for São Roque Hydroelectric Power Plant. With 285 tons each and approximately eight meters in diameter, this equipment is among the largest electric hydrogenerators ever produced by WEG.

São Roque Hydroelectric Power Plant has an installed capacity of 142 MW, which, on average, is enough to supply a city with approximately 170,000 inhabitants. The generators started commercial operation in July 2022.

Commercial and Industrial Energy Storage

Energy storage systems are used in commercial or industrial facilities, being the complete solution for storage and management of electrical energy. They can be configured to perform various functions in smart systems for generation, transmission and distribution of electric energy. The system is composed of an energy control and management solution, and it is mainly recommended for applications in systems installed behind the meter in industries, stores, shopping malls, residential condominiums and electric mobility infrastructure.

Transformers for Renewable Energy

The reliability of the transformers developed for solar plants aims at guaranteeing the supply of energy, allowing access to electricity through renewable energy generation sources. In the line of transformers for wind farms, WEG developed an extremely compact electrical and mechanical transformer design. Additionally, due to the installation layout, in which the source and the transforming unit are very close to each other, the system produces smaller losses and greater energy efficiency.

Electrical Mobility

Integrated solutions for electric vehicles

WEG continually develops innovative technologies to create electric traction systems, as well as all the electrical infrastructure necessary for the operation of electric vehicles. WEG electric traction systems can drive various road, rail and navigation vehicles, such as urban trucks and buses, vans, forklifts, trains, monorails, support vessels and tugboats.

Digital Solutions

Smart and sustainable systems

Smart systems are able to integrate different devices and machines, as well as installations and processes, promoting efficiency in decision-making and increasing operational efficiency. Smarter solutions and systems also promote more efficient use of energy resources helping reduce the carbon footprint of operations at all levels.

Automation Systems

WEG supplies completely integrated control systems that guarantee high performance of industrial processes, easy operation and productivity gains by means of state-of-the-art technology. The success of the integration of this system is in the synergy of WEG products, where motors, drives, generators, electric panels and software applications are integrated, providing the ideal solution for each requirement. The control of industrial processes requires automation systems with high reliability and uptime levels, in addition to easy asset management by the maintenance teams, extending the equipment service life and streamlining the use of resources.

WEG Transformer Fleet Management and WEG Power Transformer Specialist

WEG Transformer Fleet Management is the ideal solution to monitor online and manage the fleet of oil or dry-type transformers, enabling customers to maximize the efficiency of their operations, supporting the streamlined management of industrial plants, renewable energy generation and infrastructure. WEG Power Transformer Specialist is a digital solution used to monitor and manage power transformers that, integrated with the WEG Transformer Fleet Management platform, centralizes the signals from several sensors installed on the equipment.

WEG Motion Fleet Management

Developed to simplify and speed up the operation, maintenance and management of industrial plants, WEG Motor Fleet Management is the ideal solution for monitoring and increasing the uptime of the industrial drive fleet. Based on cloud computing technology, the performance of assets can be monitored at any time, from any part of the world. WEG Motor Fleet Management allows checking the operating status of low and medium voltage motors and drives (VSDs and soft-starters), gearboxes, gearmotors, compressors and other assets installed in any kind of industry or facility.

Ultra Low Bake (ULB) Technology for Coatings

The Ultra Low Bake (ULB) technology consists of reducing the curing time or curing temperature of powder coatings. Linked to this reduction in time or temperature (which can reach up to 35%) is the reduction in the amount of gas used in the curing ovens of customers and partners, lowering GHG emissions.

WEG partners who employ such technology in their production line, in addition to reducing environmental impact, have a significant increase in productivity and competitiveness. WEG has forty products developed for this purpose.

Material efficiency and environmental assessment of the product

In its value chain, WEG adopts initiatives in line with the principles of the circular economy, using practices that include the reuse of process residues as raw material, like stamping steel scrap used to make castings, and the adoption of programs to recover materials at the end of the product life cycle through reverse logistics and replacement plans.

The application of these concepts and practices allowed WEG to achieve a material efficiency rate close to 85%. WEG is also constantly improving and evolving the energy efficiency of its products and retrofit solutions to extend the service life of some product lines. Qualified teams work on the processes to develop new products, on the design of new lines and in the implementation of more efficient industrial processes.

WEG applies the LCA (Life Cycle Analysis) to generate the EPD (Environmental Product Declarations) according to the customers’ demands, intending, in the coming years, to expand the application of these tools.

Saiba mais sobre as ações da WEG em Sustentabilidade

Eficiência energética e automação: Móveis Videira moderniza filtro de mangas com solução WEG

Eficiência energética e automação: Móveis Videira moderniza filtro de mangas com solução WEG

Setor moveleiro avança em sustentabilidade com economia média de 32% no consumo de energia

WEG é reconhecida no Sustainability Yearbook 2026 da S&P Global

WEG é reconhecida no Sustainability Yearbook 2026 da S&P Global

Reconhecimento destaca o desempenho da companhia em sustentabilidade e reforça a consistência de sua estratégia ESG no cenário global

WEG lança FlexStrip — decapante fenol-free para manutenção de motores e componentes metálicos

WEG lança FlexStrip — decapante fenol-free para manutenção de motores e componentes metálicos

Formulação inovadora, não inflamável e de baixa toxicidade amplia segurança ocupacional e reduz custos e restrições legais na manutenção de equipamentos elétricos

WEG fornece pacote integrado de motor de rotor bobinado para aplicação em triturador no Japão

WEG fornece pacote integrado de motor de rotor bobinado para aplicação em triturador no Japão

O fornecimento fortalece a parceria de longo prazo e simplifica o comissionamento e a manutenção das operações do usuário final.

WEG fornece motores elétricos para projeto de amônia azul nos Estados Unidos

WEG fornece motores elétricos para projeto de amônia azul nos Estados Unidos

Equipamentos serão aplicados em processos com foco em sustentabilidade e baixo carbono

Grupo WEG
  • Avenida Prefeito Waldemar Grubba, 3300 - 89256-900 - Jaraguá do Sul - SC
  • Telefone: +55 47 3276 4000
  • E-mail: esg@weg.net






 

Instagram LinkedIn YouTube

 



 
WEG - Driving Efficiency and Sustainability