• Training
  • Careers
  • ‍
  • ‍
  • Login
  • English
    • Español
    • Português do Brasil

WEG Solutions for Data Center Infrastructure

The energy transition is, above all, a journey toward efficiency. It is about consuming better—with lower environmental impact and higher operational returns. Achieving this requires state-of-the-art equipment that delivers outstanding energy performance and reliability, reduced heat generation, and minimal maintenance needs. Equipment that not only operates within the data center but also communicates with smart grids and supports corporate decarbonization strategies.

Aware of both the responsibility and the opportunity, WEG seeks to play a leading role in this new chapter of the global industry. With decades of expertise in energy and industrial solutions, the company invests continuously in innovation to lead the transformation of a sector that is growing not only in consumption, but also in awareness.

WEG supports the development of reliable and scalable Data Centers through integrated electrical and electromechanical solutions, connecting utilities, substations, distribution, backup, cooling, and digital monitoring within a coordinated architecture to ensure continuous operations, facilitate expansions, and sustain high-availability and mission-critical environments.

Anatomy of a Data Center

High-voltage Substation

Responsible for receiving high-voltage power directly from the utility company. This is where the primary energy transformation takes place, ensuring a safe and continuous power supply to the data center with high performance and reliability.

Electrical Room

Handles the internal distribution of transformed energy to the various systems within the data center. It integrates transformers, panels, and protection systems that ensure energy continuity and quality at the required operating voltages.

Technical Corridor/PDU (Power Distribution Unit) Room

Area dedicated to the refined distribution of power to racks and servers. PDUs provide control, monitoring, and redundancy, optimizing energy management and minimizing risks.

Generator Room

Houses the emergency power generation systems responsible for maintaining the data center’s operation in the event of a grid failure. Robust and automated equipment ensures fast transition and continuous operation.

NOC – Network Operations Center

Control center that monitors all data center systems in real time: power, cooling, security, and data. It serves as the operational brain of the infrastructure, ensuring rapid responses and precise decision-making.

Data Hall (DH)

The main environment where servers and IT equipment are installed. Designed with advanced thermal control, electrical redundancy, and physical security, it is the heart of the digital operation of any data center.

Chilled Water Plant

Responsible for producing and distributing chilled water to cool the areas housing the servers, preventing overheating.

Fire Pump House

Dedicated facility for the fire prevention and suppression system. It contains pumps, reservoirs, and pressurization systems that ensure a rapid response to emergencies, protecting critical assets and lives.

High-voltage Substation

Turn-key substation supply. WEG has proven extensive experience, having delivered and energized over 600 substations across all voltage levels up to 550 kV.

E-houses
Oil Type Power Transformer
Disconnector

CTs and PTs (Current and potential transformers)

Measurement and protection devices for medium- and high-voltage systems, ensuring accuracy and safety.

Electrical Room

All power equipment in a Data Center is essential to ensure high business availability and minimize downtime.

Molded Case Circuit Breakers ACW
Dry-Type Transformers

Corredor Técnico e Sala de PDUs

Local destinado à distribuição refinada de energia para os racks e servidores. Os PDUs garantem controle, monitoramento e redundância, otimizando a gestão da energia e minimizando os riscos.

Painéis Elétricos

Sala dos Geradores

Todos os equipamentos de energia de um Data Center são essenciais para garantir alta disponibilidade das operações e minimizar o tempo de indisponibilidade.

Alternadores para Grupos Geradores

Sala de Monitoramento (NOC)

Os sistemas de gerenciamento de infraestrutura de Data Centers (DCIM) e de automação predial (BMS) permitem monitorar e controlar o Data Center, incluindo a capacidade de armazenamento, o tráfego de rede, o desempenho dos servidores, a iluminação, o CFTV, o ar-condicionado, bem como os sistemas de energia e refrigeração.

WEG Motion Fleet Management

Data Hall (DH)

Ambiente principal onde estão instalados os servidores e equipamentos de TI. Projetado com alto controle térmico, redundância elétrica e segurança física, é o coração da operação digital de qualquer data center.

image-not-available.jpg
Linha de pintura de pisos Epóxi
Painéis Elétricos

Central de Água Gelada

Todos os equipamentos de refrigeração são essenciais para manter as condições ambientais adequadas aos sistemas de TI e Telecomunicações do Data Center.

Painéis Totalmente Testados TTW01-QD

Casa de Combate a Incêndio

Os equipamentos de proteção contra incêndio são ferramentas e sistemas que ajudam a prevenir, detectar e combater incêndios em Data Centers.

Painéis Totalmente Testados TTW01-QD

Conheça nossas soluções

Read File

Saiba mais sobre os nossos cases

WEG e Elea Data Centers firmam parceria para aprimorar a infraestrutura de alto desempenho voltada à IA no Brasil

WEG e Elea Data Centers firmam parceria para aprimorar a infraestrutura de alto desempenho voltada à IA no Brasil

Projeto envolve o fornecimento de transformadores que alimentarão o site de alta tensão de 50 MW da Elea em São Paulo

Eletrocentros

Transformadores e TFM

Câmeras WEG

Inversor de Frequência CFW 900

Sensor de Barramentos - WEG SCAN 200

Barramento Blindado

Motores WEG para Central de Água Gelada

Motores WEG para HVAC e CAG

Institucional

Quer saber mais sobre as nossas soluções para Datacenters?

Sou um cliente do Brasil

Fale com um especialista

Sou um cliente de fora do Brasil

Fale com um especialista
WEG ELEKTRİK SANAYİ A.Ş.
  • Sales Office: Yenişehir Mahallesi, Osmanlı Bulvarı No: 11A, Esas Kurtköy Aeropark, Kat: 5, Ofis No: 28, 34912 Pendik - İstanbul / Turquia
  • Administration and Motor Campus: Kemalpaşa OSB, Ankara Asfaltı Caddesi No: 57, 35730 Kemalpaşa - İzmir / Turquia
  • Gear Systems Campus: Muradiye Mahallesi, Muradiye OSB, 7. Sokak No: 4, 45140 Yunusemre - Manisa / Turquia
  • Phone: +90 546 115 46 02
  • Email: info-tk@weg.net