WEG
  • Início
  • Produtos
    • PRODUTOS E SOLUÇÕES SUSTENTÁVEIS
    • Tecnologias e Inovação para a Transição Energética e Descarbonização
    • Cadeia de fornecimento responsável
  • Operações
    • OPERAÇÕES CIRCULARES E EFICIENTES
    • Ecoeficiência e gestão de resíduos e emissões
    • Carbono Neutro nas Operações
  • Pessoas
    • COLABORADORES E COMUNIDADES ENGAJADOS
    • Crescimento Sustentável das Comunidades
    • Bem-estar Integral, Diversidade e Inclusão
  • Governança
    • GOVERNANÇA E CONDUTA ÉTICA
    • Engajamento e Comunicação Transparente
    • Compliance e Integridade
WEG - Driving efficiency and sustainability

Engajamento e Comunicação Transparente

Relatório Anual Integrado

Para comunicar de forma transparente sobre sua gestão, desempenho, desafios e práticas de Sustentabilidade, a WEG publica anualmente seu Relatório Anual Integrado.

O Relatório segue as principais metodologias e frameworks internacionais e é verificado por terceira parte independente.

Confira os relatórios já publicados pela WEG

Materiality

The materiality process aims at helping companies identify priority sustainability topics, considering the internal and external stakeholders’ perception. In addition to being used for strategic plans, it is essential for communication aligned with the company's most relevant sustainability topics.

Attentive to the needs and expectations of its stakeholders, WEG applies its materiality process every two years.

Check here for more details on the process and WEG's current material topics

Leadership and employee development

WEG establishes in its Code of Ethics, the incentive for the self-development of employees and that investments in training are made in a fair and strategically effective manner through the evaluation of the essential and managerial competencies of our employees. We respect diversity, not admitting discrimination, prejudice or favoritism of any kind, such as ethnicity, skin color, religion, culture, age, gender, political conviction, nationality, regionality, marital status, sexual orientation, physical and intellectual condition, among others. 

In addition, as mentioned in item 7.5, we do not admit any form of moral or sexual harassment, such as insinuations, jokes, proposals or offensive physical acts. We do not accept subtle or explicit pressure to obtain favors, threats, intimidation, provocations and submission of individuals to ridicule or exclusion are also prohibited.

In 2023, we had 307 members of the CIPA (Internal Commission for the Prevention of Accidents and Harassment) elected who were trained in the CIPA course - NR05 - in which a chapter on the theme CIPA and Harassment was included. In this chapter, the contents were addressed:

  • Definition of organizational bullying
  • Knowledge of Law 14457/22
  • Rules of conduct and procedures for receiving and following up on complaints.
  • Whistleblowing Channel
  • Carry out and record other actions with employees on the topic 

In 2023, 8,528 new employees were trained in the Code of Ethics course. All other employees were trained when they joined the company and will undergo new training when there is a revision of the Code.

Performance assessment

The performance and skills assessment is a tool that aims to evaluate the performance of employees in WEG skills, highlighting their potential and opportunities for development.

It is a formal moment for feedback from the immediate superior to the employee, in which the results achieved during the year will be recognized, areas for improvement in development will be identified and career expectations will be aligned, enabling a closer relationship between the immediate superior and the employee.

The performance and skills assessment is aimed at all employees of the company (not managers) and is carried out once a year, preferably on the employee's company anniversary.

The skills assessed in all employees are: communication, knowledge, initiative, productivity, quality, and interpersonal relationships.

And for hourly employees, the following are also assessed: teamwork, attendance and punctuality, discipline, and work safety.

For monthly employees, the specific skills assessed are: creativity and innovation, customer focus, negotiation, and responsibility.

Saiba mais sobre as ações da WEG em Sustentabilidade

WEG fornece pacote integrado de motor de rotor bobinado para aplicação em triturador no Japão

WEG fornece pacote integrado de motor de rotor bobinado para aplicação em triturador no Japão

O fornecimento fortalece a parceria de longo prazo e simplifica o comissionamento e a manutenção das operações do usuário final.

WEG fornece motores elétricos para projeto de amônia azul nos Estados Unidos

WEG fornece motores elétricos para projeto de amônia azul nos Estados Unidos

Equipamentos serão aplicados em processos com foco em sustentabilidade e baixo carbono

WEG e Irmãos Cioccari impulsionam eficiência energética e sustentabilidade na produção de calcário

WEG e Irmãos Cioccari impulsionam eficiência energética e sustentabilidade na produção de calcário

Investimento contínuo em motores W22 Super Premium IR4 promove redução de consumo, confiabilidade e maior durabilidade em condições severas.

Eficiência energética no setor de criação de camarões é ampliada com WEGmotion Drives

Eficiência energética no setor de criação de camarões é ampliada com WEGmotion Drives

A eletrificação de bombas de água em fazendas de camarão permite economia de energia e redução de manutenção, reforçando a presença da WEG no mercado equatoriano.

WEG avança em programa de Eficiência Energética com modernização da Estamparia em Jaraguá do Sul

WEG avança em programa de Eficiência Energética com modernização da Estamparia em Jaraguá do Sul

Da modernização à performance: como a WEG reduziu 30% no consumo de energia.

Grupo WEG
  • Avenida Prefeito Waldemar Grubba, 3300 - 89256-900 - Jaraguá do Sul - SC
  • Telefone: +55 47 3276 4000
  • E-mail: esg@weg.net






 

Instagram LinkedIn YouTube

 



 
WEG - Driving Efficiency and Sustainability