WEG
  • Index
  • Products
    • SUSTAINABLE PRODUCTS AND SOLUTIONS
    • Technologies and Innovation for Energy Transition and Decarbonization
    • Responsible supply chain
  • Operations
    • CIRCULAR AND EFFICIENT OPERATIONS
    • Eco-efficiency and Waste and Emission Management
    • Carbon Neutral in Operations
  • People
    • ENGAGED EMPLOYEES AND COMMUNITIES
    • Sustainable Growth of the Communities
    • Comprehensive Well-being, Diversity and Inclusion
  • Governance
    • GOVERNANCE AND ETHICAL CONDUCT
    • Engagement and Transparent Communication
    • Compliance and Integrity
WEG - Driving efficiency and sustainability

Eco-efficiency and Waste and Emission Management

Circular and efficient operations

The circular economy seeks to maximize the value of resources while minimizing waste and environmental impacts. In this model, products are designed to be durable, repairable and recyclable, encouraging the reuse and recycling of materials. Instead of following the traditional linear model of production and consumption, in which products are manufactured, used and discarded, the circular economy promotes the idea of a continuous cycle, where materials are kept in use for as long as possible.

This approach not only contributes to the conservation of natural resources but also stimulates innovation, job creation and sustainable economic growth, making it essential to address today's global challenges such as climate change and resource scarcity.

Consolidating WEG's commitment, we have ISO 14,001 certifications demonstrating environmental management in the company's operations.

Programs & Practices

Residues and energy

Solid residues

WEG operations have a selective waste collection system. In this way, residues are separated and sent to recyclers of each material, enabling their appreciation and the reintroduction of such materials in different production cycles. It is important to emphasize that part of the waste generated in the operations is recycled by WEG itself, returning to the process and forming part of its products. All waste is sent to environmentally responsible companies, selected and developed by WEG's environmental management team.

See more

 

Energy

WEG has had an Energy Efficiency Policy since 2012, showing its commitment to the management of this input. This policy is deployed into actions to monitor and reduce energy consumption, which contributes to improving the environment. WEG intends to increasingly make its energy sources cleaner, renewable and sustainable.

Water, effluents and water resources

WEG monitors the water consumption of its operations and has several operational controls that ensure efficient management of this resource, thus avoiding waste and promoting conscious consumption. All effluents generated in operations are properly treated and periodically monitored in order to ensure compliance with legislation and minimize impacts on different stakeholders.

 

Part of the effluents treated in the operations are reused in the internal processes, where some effluent treatment plants enable the reuse of up to 100% of the treated effluent. We have adopted initiatives focused on reducing water consumption and effluent generation by controlling leaks, monitoring consumption and counting on the support of programs that engage all employees in this objective, such as KaizenWEG and WEG Manufacturing System.

 

Investments and expenses in the environment

Environmental investments fall into three categories:

  • Environmental control: related to treatment and disposal of residues, treatment of atmospheric and liquid emissions, environmental liability insurances, depreciation of devices and expenses with materials and maintenance.
  • Equipment: related to the purchase of equipment for environmental control.
  • Management: related to the remuneration of training staff who act in environmental management, research and development, and certification of environmental management systems.

Sustainable packaging and biodiversity preservation

We have a packaging factory, RF Reflorestadora, in Brazil. This unit produces all the wooden packaging used in our various product lines. To that end, we have our own reforestation areas that guarantee the continuous supply of wood and the preservation of this natural resource and areas of natural forests, legal reserves and permanent preservation areas that help in the preservation of the local biodiversity.

The areas comply with all legislation and legal requirements, including an area of conservation of native forests much larger than the minimum established for the legal reserve.

Furthermore, WEG promotes and supports conscious reforestation and nature conservation initiatives and invests in the afforestation of its industrial parks.

KaizenWEG

O KaizenWEG foi criado em 2016 e é o coração do sistema de gestão de melhoria contínua da WEG, o WMS, onde todos os colaboradores são incentivados a promover melhorias em seu ambiente de trabalho ou em quaisquer outras áreas da empresa, identificando desperdícios, analisando causas e participando de times multidisciplinares para a resolução de problemas. 

Sendo um dos pilares da Gestão Participativa da Companhia, desde sua criação mais de 300 mil melhorias foram implantadas, trazendo mais segurança, qualidade e produtividade, além de tornar o ambiente de trabalho cada vez mais eficiente e sustentável.

A busca coletiva pela excelência operacional e sustentabilidade em um cenário de verticalização de processos faz da gestão participativa peça chave para a potencialização de resultados da WEG.

Confira o vídeo do lançamento da nova plataforma do KaizenWEG: 

Vídeo de lançamento

 

WMS (WEG Management System)

O sistema de gestão de melhoria contínua da WEG é o WMS, que tem como principal objetivo a identificação e eliminação de perdas e desperdícios.

Os resultados são maximizados através das matrizes de priorização de segurança, qualidade, custo e emissões de GEE (gases de efeito estufa), que direcionam a ocorrência de projetos de otimização ou eliminação destes desperdícios, contribuindo para um mundo mais eficiente e sustentável.

Além das frentes de trabalho de otimização, times multidisciplinares atuam como pontos focais de melhoria contínua, trazendo inovações e disrupções nos nossos processos.

Um destes pontos focais é o pilar de Meio Ambiente e Energia, que objetiva e sistematiza a redução de impactos ambientais, atuando para reduzir ou eliminar a geração de resíduos e emissões, o consumo de recursos energéticos, limpezas químicas e insumos em geral.

Saiba mais

 

Plano de troca

Reciclagem é assunto sério para a WEG, estendido até o seu negócio. Com o programa de reaproveitamento de motores elétricos, “Plano de Troca”, a companhia concede um desconto na compra de um motor novo com rendimento superior ao exigido por lei na troca por um usado. Além do benefício financeiro aos clientes, a iniciativa garante que o motor usado com baixo nível de eficiência seja removido de uso. Depois de recolhidos pela companhia, os motores são desmontados e separados em peças para envio a recicladores credenciados e rastreados.

 

Vantagens

  • Redução do consumo de energia elétrica

  • Confiabilidade da planta

  • Redução dos custos operacionais

  • Garantia de fábrica

  • Produtos normalizados – oferecem total intercambiabilidade com motores já instalados

 

Item

2021

2022

2023

2024

Produtos vendidos que podem ser reutilizados ou reciclados* (%) – Base em peso

68

73

65

70

Produtos que foram realmente reaproveitados ou reciclados pela empresa * (%) – Base em peso

12

16

14

4

* Leva em consideração somente os produtos colocados e recolhidos no mercado Brasil

 

Investimentos em meio ambiente

Os investimentos ambientais são caracterizados em duas categorias:

Investimentos de Capital: Referentes à aquisição de equipamentos para controle ambiental.

Despesas Operacionais (R$): Referentes ao tratamento e destinação de resíduos, tratamento de emissões atmosféricas e líquidas, seguros de responsabilidade ambiental e depreciação de equipamentos, além de despesas com materiais e manutenção, além das despesas com remuneração de pessoal que atua na gestão ambiental, pesquisa e desenvolvimento e certificação de sistemas de gestão ambiental.

Abaixo o montante investido em cada categoria:

Item

2021

2022

2023

2024

Investimento de capital (R$)

1.329.000

1.788.000

1.819.000

11.141.393

Despesas Operacionais (R$)

14.684.000

17.753.000

23.509.000

33.605.910

% de cobertura (%) 70 70 70 89

 

Certificação Ambiental

Em 2024, considerando o escopo de colaboradores, 70,8% do grupo WEG estava coberto pela certificação ISO 14001.

Clique aqui para acessar nossos certificados

 

Auditorias Ambientais

A WEG possui um processo de ciclo de auditorias ambientais que cobre todas as suas operações industriais.

Dentro do seu processo anual de auditorias ambientais, a WEG garante o atendimento às legislações ambientais de todas as suas operações industriais.

 

Indicadores de Performance

Em 2023, o escopo das unidades monitoradas foi ampliado, incluindo os endereços comerciais da empresa. Dessa forma, 100% dos endereços globais da WEG agora estão contemplados nos indicadores.

 

Energia

A WEG possui Política de Eficiência Energética, desde 2012, na qual demonstra o seu compromisso com a gestão desse insumo. Essa política é desdobrada em ações para o monitoramento e a redução do consumo de energia, o que contribui para a melhoria do meio ambiente. A WEG pretende tornar, cada vez mais, suas fontes de energia mais limpas, renováveis e sustentáveis.

Consumo total de energia

Unidade

2021

2022

2023

2024

Consumo total de energia Não-Renovável

MWh

535.599

510.110

454.702

212.113

Consumo total de energia Renovável

MWh

57.801

88.904

129.202

427.398

Consumo total de energia (Não-Renovável + Renovável)

MWh

593.400

599.014

583.904

 639.511

Dados de cobertura (%)

Em relação à funcionários

100 100 100 100

Aquisição de energia renovável

Em 2024, a WEG garantiu que 66,8% do consumo de energia fosse proveniente de fontes renováveis com garantia de origem por meio autoprodução, compra de certificados de energia renovável (I-REC) e contratos bilaterais.

Emissões Atmosféricas

A WEG realiza o monitoramento das emissões atmosférica relacionadas aos compostos orgânicos voláteis. Abaixo segue o resultado das emissões relacionadas aos equipamentos monitorados nos últimos anos.

 

Item

2019

2020

2021

2022

2023

2024

Emissões de compostos orgânicos voláteis - VOC (t/ano)

93,5 135,2 114,5

139,3

191,3 241,3

Taxa de cobertura (%)

56

56

56

61

72

61

 

Violações Ambientais

Uma das principais prioridades da WEG é a conformidade com a legislação ambiental aplicável às suas operações. Nos últimos 4 anos, não houve evidências de multas ambientais significativas aplicadas aos negócios da WEG.

Saiba mais sobre as ações da WEG em Sustentabilidade

WEG fornece pacote integrado de motor de rotor bobinado para aplicação em triturador no Japão

WEG fornece pacote integrado de motor de rotor bobinado para aplicação em triturador no Japão

O fornecimento fortalece a parceria de longo prazo e simplifica o comissionamento e a manutenção das operações do usuário final.

WEG fornece motores elétricos para projeto de amônia azul nos Estados Unidos

WEG fornece motores elétricos para projeto de amônia azul nos Estados Unidos

Equipamentos serão aplicados em processos com foco em sustentabilidade e baixo carbono

WEG e Irmãos Cioccari impulsionam eficiência energética e sustentabilidade na produção de calcário

WEG e Irmãos Cioccari impulsionam eficiência energética e sustentabilidade na produção de calcário

Investimento contínuo em motores W22 Super Premium IR4 promove redução de consumo, confiabilidade e maior durabilidade em condições severas.

Eficiência energética no setor de criação de camarões é ampliada com WEGmotion Drives

Eficiência energética no setor de criação de camarões é ampliada com WEGmotion Drives

A eletrificação de bombas de água em fazendas de camarão permite economia de energia e redução de manutenção, reforçando a presença da WEG no mercado equatoriano.

WEG avança em programa de Eficiência Energética com modernização da Estamparia em Jaraguá do Sul

WEG avança em programa de Eficiência Energética com modernização da Estamparia em Jaraguá do Sul

Da modernização à performance: como a WEG reduziu 30% no consumo de energia.

Grupo WEG
  • Avenida Prefeito Waldemar Grubba, 3300 - 89256-900 - Jaraguá do Sul - SC
  • Telefone: +55 47 3276 4000
  • E-mail: esg@weg.net






 

Instagram LinkedIn YouTube

 



 
WEG - Driving Efficiency and Sustainability