Does the dosing nozzle make the painter's job easier?
The W-Acqua line doser allows the operator to better control the volume of paint that will leave the package to carry out the weighing of the mixings on the scale, thus avoiding errors that may occur when carrying out the weighing of colors. 
How is W-Acqua less harmful to health? How is it different from other solvent-based products?
Water-based automotive paints are recognized worldwide for their quality and low emission of VOC's (Volatile Organic Compounds), it is good for the environment and excellent for the applicator, who is not exposed to compounds harmful to health and strong scents from solvents. By using water in its composition and as a diluent, the W-Acqua system does not offer the same risks as the conventional system.
What are the dimensions of WEG Transformer Scan?

The dimensions (length x width x heigth) of the product are: 291.7 x 267.7 x 100.2 mm or 11.48 x 10.54 x 3.95 in

I forgot my password. How can I recover it?

You need to remember the email address you used on your account to perform automatic recovery. Just go to https://tfm.wnology.io/ and click on the "Forgot your password?" link.

Enter your email and click on "Request password reset". Open the email with the title "Request to Reset Password" and click on the link in the body of the message, you will be redirected to a page where you can create a new password.

How do I connect my transformer to the Transformer Fleet Management portal?

If you have not created a plant yet, go to the "Register and Edit" menu > "System" and click on the "+Plant" button, fill in the data and click on "Save". After this step, it is possible to add a new transformer to your plant.

If you want to add a new transformer to an existing plant, go to the "Register and Edit" menu > "Devices" and click on the "+Add" button, then select the type of transformer and fill in the data, then click on "Save".

  • 1
  • ...
  • 264
  • 265
  • 266
  • ...
  • 272
WEG AUSTRALIA PTY LTD
  • 14 Lakeview Drive, Scoresby 3179 - Victoria / Australia
  • Phone: + 61 3 9765 4600
  • Email: info-au@weg.net