Through the company’s strategic direction towards its business model, WEG offers in all its business units more efficient solutions and products with lower environmental impact, such as renewable energy (solar, wind), electric mobility, energy efficiency, among others. WEG develops products considering strict risk criteria related to health and safety. During the development phase, analyses are applied, such as: Quality Function Deployment (QFD) and Risk Assessment.
WEG applies a certified quality management system, based on external requirements and the requirements of our customers.
Below are some highlights considering the variety of products and solutions the company provides to the market through its different business units.
Efficient and compact solution thar delivers high performance with reduced size and weight in comparison to the previous line (up to 25% higher power density – kW/kg) and its competitors. Therefore, it makes rational use of raw materials in the manufacture of motors and reduces the potential effects of their transformation, cutting down GHG emissions by about 15% in comparison to the previous line.
High-tech VSD for driving and controlling three-phase induction and permanent magnet motors. Thanks to its technology, this VSD model provides energy savings, safety, increased productivity and quality in the process network in which it is implemented. The CFW900, together with permanent magnet motors, offers the highest energy efficiency solution on the market. The new HMI with Bluetooth® connectivity is ideal for panel builders and repair shops, enabling programming, monitoring, parameter backup and other functionalities via tablets or smartphones.
For application in front load washing machines, it delivers a 60% improvement in the performance of the operating cycle and, consequently, a reduction of GHG emissions during the operation phase. This line currently represents 20% of the volume sold by WEG for front load washing machines.
In July 2022, WEG announced the release of a new wind turbine platform with 7 MW power and 172 meters of blade rotor diameter. This wind turbine will become the largest machine in operation in the Brazilian market. More powerful and efficient, the new model brings greater generation to wind projects.
WEG established itself as one of the main suppliers of products and solutions for solar plants in Brazil, bringing efficiency that drives sustainability in cities, industries, agribusiness and homes across the country. WEG has a vast portfolio of products for all the stages of photovoltaic solar generation projects, with solutions for the energy conversion and internal distribution system, from the plant to the point of connection to the electrical system through high voltage substations.
A WEG foi selecionada para fornecer os geradores da UHE São Roque, situada em Vargem/SC. Os geradores são uma das partes mais importantes que compõem o empreendimento para a UHE São Roque. Com 285 toneladas cada e aproximadamente oito metros de diâmetro, estes equipamentos estão entre os maiores hidrogeradores elétricos já produzidos pela WEG.
A UHE São Roque tem potência instalada de 142 MW que, em média, é suficiente para abastecer uma cidade com aproximadamente 170 mil habitantes. Os geradores entraram em operação comercial em julho de 2022.
Os sistemas de armazenamento de energia são utilizados em instalações comerciais ou industriais, sendo a solução completa para armazenamento e gerenciamento de energia elétrica armazenada, podendo ser configurados para desempenhar várias funções em sistemas inteligentes de geração, transmissão e distribuição de energia elétrica. O sistema é composto por uma solução de controle e gestão energética, sendo indicado principalmente para aplicações em sistemas instalados atrás do medidor em indústrias, comércios, shopping centers, condomínios residenciais e infraestrutura de mobilidade elétrica.
A confiabilidade dos transformadores desenvolvidos para usinas solares tem como objetivo a garantia do fornecimento de energia, permitindo acesso à eletricidade por meio de fontes de geração de energia renovável. Na linha de transformadores para usinas eólicas, a WEG desenvolveu projeto elétrico e mecânico do transformador extremamente compacto. Adicionalmente, pela configuração da instalação, na qual a fonte e a unidade transformadora encontram-se muito próximas entre si, o sistema possibilita menos perdas e mais eficiência energética.
A WEG desenvolve continuamente tecnologias inovadoras para criar sistemas de tração elétrica, bem como toda a infraestrutura elétrica necessária para operação de veículos elétricos. Os sistemas de tração elétrica WEG podem ser aplicados em diversos veículos rodoviários, ferroviários e de navegação, tais como caminhões e ônibus urbanos, furgões, empilhadeiras elétricas, trens, monotrilhos, navios de suporte e rebocadores.
Sistemas inteligentes são capazes de integrar os mais variados dispositivos e máquinas, bem como instalações e processos, promovendo eficiência na tomada de decisão e aumento da eficiência operacional. Soluções e sistemas mais inteligentes também promovem a utilização mais eficiente de recursos energéticos ajudando a reduzir pegada de carbono das operações em todos os níveis.
A WEG fornece sistemas de controle completamente integrados, garantindo ainda alto desempenho dos processos industriais, facilidade de operação e ganho de produtividade por meio de tecnologia de ponta. O sucesso da integração desse sistema está na sinergia dos produtos WEG, na qual motores, drives, geradores, painéis elétricos e softwares são integrados, fornecendo a solução ideal para cada necessidade. O controle de processos industriais exige sistemas de automação com elevado grau de confiabilidade e disponibilidade, além de facilidade para equipes de manutenção no gerenciamento de ativos, estendendo a vida dos equipamentos e racionalizando o uso de recursos.
WEG Transformer Fleet Management es la solución ideal para monitorear online y supervisar la flota de transformadores a aceite o del tipo seco, posibilitando que los clientes maximicen la eficiencia de sus operaciones, en apoyo a la gestión optimizada de plantas industriales, de generación de energías renovables y de infraestructura. Por otro lado, la solución WEG Power Transformer Specialist es una solución digital aplicada en el monitoreo y en la gestión de transformadores de potencia que, integrada a la plataforma WEG Transformer Fleet Management, centraliza las señales de una serie de sensores instalados en el equipo.
Desarrollado para llevar más practicidad y agilidad a la operación, en el mantenimiento y en la gestión de plantas industriales, el WEG Motion Fleet Management es la solución ideal para monitorear y elevar la disponibilidad de la flota de accionamiento industrial. Basado en tecnología “cloud computing”, el monitoreo de los activos puede ser seguido en cualquier momento y desde cualquier parte del mundo. Con el Motion Fleet Management es posible conocer el estado operacional de motores y drives (convertidores y arrancadores suaves) de baja y media tensión, reductores, motorreductores, compresores, entre otros activos que estén aplicados en cualquier tipo de industria o instalación
La tecnología Ultra Low Bake (ULB) consiste en reducir el tiempo de cura o la temperatura de cura de las pinturas en polvo. Asociado a esa reducción de tiempo o temperatura (que puede llegar a 35% de reducción), reduciendo la cantidad de gas que es utilizada en los hornos de cura de sus clientes y aliados, así como reduciendo las emisiones de GEE.
Los aliados de WEG que poseen esa tecnología en su línea de producción, además de la reducción del impacto ambiental, tienen aumento significativo de productividad y en su competitividad. WEG cuanta con cuarenta productos desarrollados con esa finalidad.
In its value chain, WEG adopts initiatives in line with the principles of the circular economy, using practices that include the reuse of process residues as raw material, like stamping steel scrap used to make castings, and the adoption of programs to recover materials at the end of the product life cycle through reverse logistics and replacement plans.
The application of these concepts and practices allowed WEG to achieve a material efficiency rate close to 85%. WEG is also constantly improving and evolving the energy efficiency of its products and retrofit solutions to extend the service life of some product lines. Qualified teams work on the processes to develop new products, on the design of new lines and in the implementation of more efficient industrial processes.
WEG applies the LCA (Life Cycle Analysis) to generate the EPD (Environmental Product Declarations) according to the customers’ demands, intending, in the coming years, to expand the application of these tools.