• Formation
  • Carrières
  • ‍
  • ‍
  • Login
  • Français
    • English
    • Español
    • Português do Brasil
  • Index
  • Products
  • Services
  • Operation and Maintenance
  1. Page d'accueil
  2. Wind Power Solutions

Aiming to enhance performance and reliability?
Rely on WEG’s proven solutions!

WEG offers a comprehensive portfolio of solutions engineered for maximum operational reliability and superior lifecycle performance. Our offerings include wind turbines, generators and transformers, each carefully designed to meet the rigorous demands of today’s wind energy industry.

WEG is more than a supplier. We are your strategic partner in ensuring the success of your renewable projects at every phase, from planning through operation.

Trust in WEG’s decades of expertise and commitment to continuous improvement to advance and secure the long-term success of your wind assets!

Learn more about our products and solutions

Wind Turbines - AGW172 / 7.X
Wind Turbines - AGW147 / 4.2
Wind Generators
Power Transformers (up to 50 MVA)
Power Transformers (up to 500 MVA)
Medium Distribution Transformer (up to 3,000 kVA)
Conventional Substation
Disconnector

Wind Turbine - AGW172 / 7.X

The AGW172/7.X wind turbine embodies WEG’s commitment to advanced engineering and operational excellence.

With a 7 MW rated power and a 172-meter rotor, it features a medium-speed gearbox and a permanent magnet synchronous generator for optimized energy conversion, along with a full-power converter for smooth and stable grid interconnection.

Engineered for superior reliability and compliance with the strictest international standards, this platform delivers clean energy with enhanced operational availability and simplified maintenance.

AGW 172/7.X is your choice for long-term asset value in wind energy projects!

Stay updated with WEG's news in Wind Energy

Innovative partnership between WEG, Petrobras, and Statkraft brings the largest onshore wind turbine in the Americas into operation

Innovative partnership between WEG, Petrobras, and Statkraft brings the largest onshore wind turbine in the Americas into operation

Modernization project of the Brotas de Macaúbas Complex will increase efficiency and reinforce the pioneering spirit of the venture with a 7MW installed capacity turbine

WEG and Statkraft Sign Partnership for Implementation of the Largest Onshore Wind Turbine Produced in Brazil

WEG and Statkraft Sign Partnership for Implementation of the Largest Onshore Wind Turbine Produced in Brazil

The partnership will promote the installation of a wind turbine in the Brotas de Macaúbas Wind Complex in Bahia

WEG and Petrobras sign a partnership agreement for the development of the largest wind turbine in the country

WEG and Petrobras sign a partnership agreement for the development of the largest wind turbine in the country

The equipment will have a capacity of 7 MW and will be the first of its kind in Brazil

WEG confirma participação no maior evento de energia eólica da América Latina

WEG confirma participação no maior evento de energia eólica da América Latina

A feira Brazil Windpower acontece de 12 a 14 setembro no São Paulo Expo

WEG supplies motors to a platform to test and validate wind turbine technology

WEG supplies motors to a platform to test and validate wind turbine technology

Equipment will be part of the largest and most powerful powertrain and gearbox test bench in the world

WEG announces agreement with 2W Ecobank for self-production of wind power

WEG announces agreement with 2W Ecobank for self-production of wind power

The initiative will guarantee the supply of renewable energy in five industrial facilities of the Company in Brazil

WEG and Alupar sign agreement for self-production of wind power

WEG and Alupar sign agreement for self-production of wind power

Project will reinforce the energy supply of four industrial plants and the Company's commitment to sustainability

WEG Transformers and Shunt Reactors are supplied for a wind farm in northern Colombia

WEG Transformers and Shunt Reactors are supplied for a wind farm in northern Colombia

The equipment is part of a wind farm project with 492MW power capacity

WEG to launch a 7 MW wind turbine

WEG to launch a 7 MW wind turbine

The prototype should be ready for operation by 2024 and regular production to start in 2025

WEG supplies product package for a solar and wind power plant in Brazil

WEG supplies product package for a solar and wind power plant in Brazil

Five solar and wind power projects will be benefited by this product supply.

WEG and Engie Brasil Energia complete installation of the first national wind turbine

WEG and Engie Brasil Energia complete installation of the first national wind turbine

Wind turbine is part of the project for the first National Wind Turbine, which is intended to develop national technology and production chain for the manufacture and installation of large size equipment in the country

WEG joins a Business Mission to India

WEG joins a Business Mission to India

The "India - Brazil Business Forum”, was organized by the Brazilian Export and Investment Promotion Agency (Apex-Brasil) and took place in New Delhi, India.

WEG signs an agreement to supply wind turbines to Aliança Energia´s Wind Farms

WEG signs an agreement to supply wind turbines to Aliança Energia´s Wind Farms

The entire agreement includes the construction of four wind farms, in a total amount of 180.6 megawatts (MW) of installed capacity

WEG anuncia la entrada en el mercado eólico Hindú

La compañía tiene la intención de ajustar su fábrica de motores y generadores, en el estado de Tamil Nadu, cerca de Bangalore, para tambi...

WEG suministra paquete eléctrico completo para un complejo de energía eólica

Nuevo complejo eólico generará 230 MVA, potencia suficiente para abastecer a 400.000 hogares, lo que equivale a una ciudad con más de un ...

WEG Auxilia en la Generación de Energía Hidroeléctrica para Windsor Castle

La Eficiencia es el objetivo clave para esta aplicación, así como el hecho de que la instalación tenga un período de retorno de inversión...

WEG establishes a Joint Venture to produce wind turbines

WEG and the Spanish company - M. Torres Olvega Industrial (MTOI) – have established a Joint Venture for the manufacturing of wind turbine...

WEG MEXICO, S.A. DE C.V
  • Carretera Jorobas - Tula Km 3.5, Manzana 5, Lote 1, Fraccionamiento Parque Industrial Huehuetoca, Municipio de Huehuetoca - 54680 - CD. de México y Área Metropolitana / Mexique
  • Téléphone: +52 55 5321 4275 (Ventas Nacionales) / +52 55 5321 4210 (Ventas Internacionales)
  • Courriel: info-mx@weg.net
  • para centroamerica contacte: rfq-wmx@weg.net