WEG
  • Index
  • Products
    • SUSTAINABLE PRODUCTS AND SOLUTIONS
    • Technologies and Innovation for Energy Transition and Decarbonization
    • Responsible supply chain
  • Operations
    • CIRCULAR AND EFFICIENT OPERATIONS
    • Eco-efficiency and Waste and Emission Management
    • Carbon Neutral in Operations
  • People
    • ENGAGED EMPLOYEES AND COMMUNITIES
    • Sustainable Growth of the Communities
    • Comprehensive Well-being, Diversity and Inclusion
  • Governance
    • GOVERNANCE AND ETHICAL CONDUCT
    • Engagement and Transparent Communication
    • Compliance and Integrity
WEG - Driving efficiency and sustainability
 

Technologies and Innovations for Energy Transition and Decarbonization

 

Through the company’s strategic direction towards its business model, WEG offers in all its business units more efficient solutions and products with lower environmental impact, such as renewable energy (solar, wind), electric mobility, energy efficiency, among others. WEG develops products considering strict risk criteria related to health and safety. During the development phase, analyses are applied, such as: Quality Function Deployment (QFD) and Risk Assessment.

Quality Management System

WEG applies a certified quality management system, based on external requirements and the requirements of our customers.

See more

Below are some highlights considering the variety of products and solutions the company provides to the market through its different business units.

Energy and Industrial Efficiency

W51 HD Motor (High Density)

Efficient and compact solution thar delivers high performance with reduced size and weight in comparison to the previous line (up to 25% higher power density – kW/kg) and its competitors. Therefore, it makes rational use of raw materials in the manufacture of motors and reduces the potential effects of their transformation, cutting down GHG emissions by about 15% in comparison to the previous line.

VSD for Motors

High-tech VSD for driving and controlling three-phase induction and permanent magnet motors. Thanks to its technology, this VSD model provides energy savings, safety, increased productivity and quality in the process network in which it is implemented. The CFW900, together with permanent magnet motors, offers the highest energy efficiency solution on the market. The new HMI with Bluetooth® connectivity is ideal for panel builders and repair shops, enabling programming, monitoring, parameter backup and other functionalities via tablets or smartphones.

BLDC Motor Line (Brushless DC)

For application in front load washing machines, it delivers a 60% improvement in the performance of the operating cycle and, consequently, a reduction of GHG emissions during the operation phase. This line currently represents 20% of the volume sold by WEG for front load washing machines.

Renewable Energy

Wind Power

In July 2022, WEG announced the release of a new wind turbine platform with 7 MW power and 172 meters of blade rotor diameter. This wind turbine will become the largest machine in operation in the Brazilian market. More powerful and efficient, the new model brings greater generation to wind projects.

Solar Power

WEG established itself as one of the main suppliers of products and solutions for solar plants in Brazil, bringing efficiency that drives sustainability in cities, industries, agribusiness and homes across the country. WEG has a vast portfolio of products for all the stages of photovoltaic solar generation projects, with solutions for the energy conversion and internal distribution system, from the plant to the point of connection to the electrical system through high voltage substations.

Hydroelectric Generation

WEG was selected to supply the generators for São Roque Hydroelectric Power Plant, located in the city of Vargem-SC. The generators are one of the most important parts of the enterprise for São Roque Hydroelectric Power Plant. With 285 tons each and approximately eight meters in diameter, this equipment is among the largest electric hydrogenerators ever produced by WEG.

São Roque Hydroelectric Power Plant has an installed capacity of 142 MW, which, on average, is enough to supply a city with approximately 170,000 inhabitants. The generators started commercial operation in July 2022.

Commercial and Industrial Energy Storage

Energy storage systems are used in commercial or industrial facilities, being the complete solution for storage and management of electrical energy. They can be configured to perform various functions in smart systems for generation, transmission and distribution of electric energy. The system is composed of an energy control and management solution, and it is mainly recommended for applications in systems installed behind the meter in industries, stores, shopping malls, residential condominiums and electric mobility infrastructure.

Transformadores para Energías Renovables

La confiabilidad de los transformadores desarrollados para centrales solares tiene como objetivo la garantía del suministro de energía, permitiendo acceso a electricidad por medio de fuentes de generación de energía renovable. En la línea de transformadores para centrales eólicas, WEG desarrolló el proyecto eléctrico y mecánico del transformador extremadamente compacto. Adicionalmente, por la configuración de la instalación, en la cual la fuente y la unidad transformadora se encuentran muy cerca entre sí, el sistema posibilita menos pérdidas y más eficiencia energética.

Movilidad Eléctrica

Soluciones integradas para vehículos eléctricos

WEG desarrolla continuamente tecnologías innovadoras para crear sistemas de tracción eléctrica, así como toda la infraestructura eléctrica necesaria para operación de vehículos eléctricos. Los sistemas de tracción eléctrica WEG pueden ser aplicados en diversos vehículos carreteros, ferroviarios y de navegación, tales como camiones y ómnibus urbanos, furgones, apiladoras eléctricas, trenes, monorrieles, barcos de soporte y remolcadores.

Soluciones digitales

Sistemas inteligentes y sustentables

Los sistemas inteligentes son capaces de integrar los más variados dispositivos y máquinas, así como instalaciones y procesos, promoviendo eficiencia en la toma de decisión y aumento de la eficiencia operacional. Soluciones y sistemas más inteligentes también promueven la utilización más eficiente de recursos energéticos, ayudando a reducir la huella de carbono de las operaciones, en todos los niveles.

Sistemas de Automatización

WEG suministra sistemas de control completamente integrados, garantizando también alto desempeño de los procesos industriales, facilidad de operación y ganancia de productividad, por medio de tecnología de punta. El éxito de la integración de este sistema está en la sinergia de los productos WEG, en la cual motores, drives, generadores, tableros eléctricos y software son integrados, suministrando la solución ideal para cada necesidad. El control de procesos industriales exige sistemas de automatización con elevado grado de confiabilidad y disponibilidad, además de facilidad para equipos de mantenimiento en la gestión de activos, extendiendo la vida de los equipos y racionalizando el uso de recursos.

WEG Transformer Fleet Management and WEG Power Transformer Specialist

WEG Transformer Fleet Management es la solución ideal para monitorear online y supervisar la flota de transformadores a aceite o del tipo seco, posibilitando que los clientes maximicen la eficiencia de sus operaciones, en apoyo a la gestión optimizada de plantas industriales, de generación de energías renovables y de infraestructura. Por otro lado, la solución WEG Power Transformer Specialist es una solución digital aplicada en el monitoreo y en la gestión de transformadores de potencia que, integrada a la plataforma WEG Transformer Fleet Management, centraliza las señales de una serie de sensores instalados en el equipo.

WEG Motion Fleet Management

Desarrollado para llevar más practicidad y agilidad a la operación, en el mantenimiento y en la gestión de plantas industriales, el WEG Motion Fleet Management es la solución ideal para monitorear y elevar la disponibilidad de la flota de accionamiento industrial. Basado en tecnología “cloud computing”, el monitoreo de los activos puede ser seguido en cualquier momento y desde cualquier parte del mundo. Con el Motion Fleet Management es posible conocer el estado operacional de motores y drives (convertidores y arrancadores suaves) de baja y media tensión, reductores, motorreductores, compresores, entre otros activos que estén aplicados en cualquier tipo de industria o instalación

Tecnología Ultra Low Bake (ULB) para Pinturas

La tecnología Ultra Low Bake (ULB) consiste en reducir el tiempo de cura o la temperatura de cura de las pinturas en polvo. Asociado a esa reducción de tiempo o temperatura (que puede llegar a 35% de reducción), reduciendo la cantidad de gas que es utilizada en los hornos de cura de sus clientes y aliados, así como reduciendo las emisiones de GEE.

Los aliados de WEG que poseen esa tecnología en su línea de producción, además de la reducción del impacto ambiental, tienen aumento significativo de productividad y en su competitividad. WEG cuanta con cuarenta productos desarrollados con esa finalidad.

Eficiencia material y evaluación ambiental del producto

WEG adopta, en su cadena de valor, iniciativas que están alineadas a los principios de la economía circular, a través de prácticas como reinserción de residuos de los procesos como materias primas, como por ejemplo chatarra de acero de la estampería, para fabricación de piezas fundidas, adopción de programas de recuperación de materiales en el fin del ciclo de vida de productos, a través de la logística reversa y de planes de cambio.

La aplicación de esos conceptos y prácticas permitieron a WEG alcanzar un índice de eficiencia material de cerca de 85%. WEG también está en constante mejora y evolución de la eficiencia energética de sus productos y de soluciones de retrofit para la extensión de la vida útil de algunas líneas de productos. Equipos cualificados actúan tanto en los procesos de desarrollo de nuevos productos y en la concepción de nuevas líneas, como en la implantación de procesos industriales más eficientes.

WEG aplica el ACV (Análisis de Ciclo de Vida), generando los EPDs (Environmental Product Declarations) conforme las demandas de los clientes, con el objetivo, en los próximos años, de ampliar la aplicación de esas herramientas.

Sepa más sobre las acciones de WEG en Sustentabilidad

WEG se destaca con tres casos en el 3.er Premio Paint & Pintura de Innovación y Sostenibilidad

WEG se destaca con tres casos en el 3.er Premio Paint & Pintura de Innovación y Sostenibilidad

El reconocimiento destaca iniciativas en pinturas líquidas, pinturas en polvo y sostenibilidad desarrolladas por WEG en Brasil y Argentina

WEG suministra un motor de media tensión diseñado a medida para proyecto en el Puerto de Róterdam

WEG suministra un motor de media tensión diseñado a medida para proyecto en el Puerto de Róterdam

El motor W50 diseñado a medida combina un diseño compacto, eficiencia IE4 y alta confiabilidad para respaldar una de las mayores iniciativas de captura de carbono de Europa

WEG fabrica un motor para la circulación de aire con tecnología 100% brasileña

WEG fabrica un motor para la circulación de aire con tecnología 100% brasileña

El resultado es un mayor ahorro de energía para aires acondicionados, climatizadores y ventiladores

WEG Pinturas en Argentina adopta energía 100% renovable en colaboración con 360Energy

WEG Pinturas en Argentina adopta energía 100% renovable en colaboración con 360Energy

El proyecto refuerza el compromiso de WEG con la descarbonización de la industria y el uso de fuentes limpias.

WEG ofrece soluciones de acabado técnico para entornos de salud

WEG ofrece soluciones de acabado técnico para entornos de salud

La tecnología de pinturas en polvo combina protección, seguridad operativa y sostenibilidad en aplicaciones hospitalarias

Grupo WEG
  • Avenida Prefeito Waldemar Grubba, 3300 - 89256-900 - Jaraguá do Sul - SC
  • Teléfono: +55 47 3276 4000
  • E-mail: esg@weg.net






 

Instagram LinkedIn YouTube

 



 
WEG - Driving Efficiency and Sustainability