WEG
  • Index
  • Products
    • SUSTAINABLE PRODUCTS AND SOLUTIONS
    • Technologies and Innovation for Energy Transition and Decarbonization
    • Responsible supply chain
  • Operations
    • CIRCULAR AND EFFICIENT OPERATIONS
    • Eco-efficiency and Waste and Emission Management
    • Carbon Neutral in Operations
  • People
    • ENGAGED EMPLOYEES AND COMMUNITIES
    • Sustainable Growth of the Communities
    • Comprehensive Well-being, Diversity and Inclusion
  • Governance
    • GOVERNANCE AND ETHICAL CONDUCT
    • Engagement and Transparent Communication
    • Compliance and Integrity
WEG - Driving efficiency and sustainability
 

Technologies and Innovations for Energy Transition and Decarbonization

 

Through the company’s strategic direction towards its business model, WEG offers in all its business units more efficient solutions and products with lower environmental impact, such as renewable energy (solar, wind), electric mobility, energy efficiency, among others. WEG develops products considering strict risk criteria related to health and safety. During the development phase, analyses are applied, such as: Quality Function Deployment (QFD) and Risk Assessment.

Quality Management System

WEG applies a certified quality management system, based on external requirements and the requirements of our customers.

See more

Below are some highlights considering the variety of products and solutions the company provides to the market through its different business units.

Energy and Industrial Efficiency

W51 HD Motor (High Density)

Efficient and compact solution thar delivers high performance with reduced size and weight in comparison to the previous line (up to 25% higher power density – kW/kg) and its competitors. Therefore, it makes rational use of raw materials in the manufacture of motors and reduces the potential effects of their transformation, cutting down GHG emissions by about 15% in comparison to the previous line.

VSD for Motors

High-tech VSD for driving and controlling three-phase induction and permanent magnet motors. Thanks to its technology, this VSD model provides energy savings, safety, increased productivity and quality in the process network in which it is implemented. The CFW900, together with permanent magnet motors, offers the highest energy efficiency solution on the market. The new HMI with Bluetooth® connectivity is ideal for panel builders and repair shops, enabling programming, monitoring, parameter backup and other functionalities via tablets or smartphones.

Linha de Motores BLDC (Brushless DC

Para aplicação em máquinas de lavar roupas front load, apresenta uma melhoria de 60% de rendimento do ciclo de funcionamento e, consequentemente, redução de GEE durante a fase de utilização. Esta linha representa atualmente 20% do volume comercializado pela WEG para máquinas de lavar front load.

Energias Renováveis

Energia Eólica

Em julho de 2022, a WEG anunciou o lançamento de uma nova plataforma de aerogeradores com potência de 7 MW e 172 metros de diâmetro de rotor das pás. Esse aerogerador se tornará a maior máquina em operação no mercado brasileiro. Mais potente e eficiente, o novo modelo traz maior geração para os projetos eólicos.

Energia Solar

A WEG se consolida como um dos principais fornecedores de produtos e soluções para usinas solares do Brasil levando a eficiência que impulsiona a sustentabilidade nas cidades, nas indústrias, no agronegócio e nos lares de todo o país. A WEG possui um vasto portfólio de produtos para projetos de geração solar fotovoltaica em todas as etapas do empreendimento, com soluções para o sistema de conversão de energia e de distribuição interna da planta até o ponto de conexão com o sistema elétrico por meio das subestações de alta tensão.

Geração Hidrelétrica

A WEG foi selecionada para fornecer os geradores da UHE São Roque, situada em Vargem/SC. Os geradores são uma das partes mais importantes que compõem o empreendimento para a UHE São Roque. Com 285 toneladas cada e aproximadamente oito metros de diâmetro, estes equipamentos estão entre os maiores hidrogeradores elétricos já produzidos pela WEG.

A UHE São Roque tem potência instalada de 142 MW que, em média, é suficiente para abastecer uma cidade com aproximadamente 170 mil habitantes. Os geradores entraram em operação comercial em julho de 2022.

Armazenamento de Energia Comercial e Industrial

Os sistemas de armazenamento de energia são utilizados em instalações comerciais ou industriais, sendo a solução completa para armazenamento e gerenciamento de energia elétrica armazenada, podendo ser configurados para desempenhar várias funções em sistemas inteligentes de geração, transmissão e distribuição de energia elétrica. O sistema é composto por uma solução de controle e gestão energética, sendo indicado principalmente para aplicações em sistemas instalados atrás do medidor em indústrias, comércios, shopping centers, condomínios residenciais e infraestrutura de mobilidade elétrica.

Transformadores para Energias Renováveis

A confiabilidade dos transformadores desenvolvidos para usinas solares tem como objetivo a garantia do fornecimento de energia, permitindo acesso à eletricidade por meio de fontes de geração de energia renovável. Na linha de transformadores para usinas eólicas, a WEG desenvolveu projeto elétrico e mecânico do transformador extremamente compacto. Adicionalmente, pela configuração da instalação, na qual a fonte e a unidade transformadora encontram-se muito próximas entre si, o sistema possibilita menos perdas e mais eficiência energética.

Mobilidade Elétrica

Soluções integradas para veículos elétricos

A WEG desenvolve continuamente tecnologias inovadoras para criar sistemas de tração elétrica, bem como toda a infraestrutura elétrica necessária para operação de veículos elétricos. Os sistemas de tração elétrica WEG podem ser aplicados em diversos veículos rodoviários, ferroviários e de navegação, tais como caminhões e ônibus urbanos, furgões, empilhadeiras elétricas, trens, monotrilhos, navios de suporte e rebocadores.

Soluções Digitais

Sistemas inteligentes e sustentáveis

Sistemas inteligentes são capazes de integrar os mais variados dispositivos e máquinas, bem como instalações e processos, promovendo eficiência na tomada de decisão e aumento da eficiência operacional. Soluções e sistemas mais inteligentes também promovem a utilização mais eficiente de recursos energéticos ajudando a reduzir pegada de carbono das operações em todos os níveis.

Sistemas de Automação

A WEG fornece sistemas de controle completamente integrados, garantindo ainda alto desempenho dos processos industriais, facilidade de operação e ganho de produtividade por meio de tecnologia de ponta. O sucesso da integração desse sistema está na sinergia dos produtos WEG, na qual motores, drives, geradores, painéis elétricos e softwares são integrados, fornecendo a solução ideal para cada necessidade. O controle de processos industriais exige sistemas de automação com elevado grau de confiabilidade e disponibilidade, além de facilidade para equipes de manutenção no gerenciamento de ativos, estendendo a vida dos equipamentos e racionalizando o uso de recursos.

WEG Transformer Fleet Management and WEG Power Transformer Specialist

O WEG Transformer Fleet Management é a solução ideal para monitorar on-line e gerir a frota de transformadores a óleo ou do tipo seco, possibilitando que os clientes maximizem a eficiência das suas operações, em apoio à gestão otimizada de plantas industriais, de geração de energias renováveis e de infraestrutura. Já a solução WEG Power Transformer Specialist é uma solução digital aplicada no monitoramento e na gestão de transformadores de potência que, integrada à plataforma WEG Transformer Fleet Management, centraliza os sinais de uma série de sensores instalados no equipamento.

WEG Motion Fleet Management

Developed to simplify and speed up the operation, maintenance and management of industrial plants, WEG Motor Fleet Management is the ideal solution for monitoring and increasing the uptime of the industrial drive fleet. Based on cloud computing technology, the performance of assets can be monitored at any time, from any part of the world. WEG Motor Fleet Management allows checking the operating status of low and medium voltage motors and drives (VSDs and soft-starters), gearboxes, gearmotors, compressors and other assets installed in any kind of industry or facility.

Ultra Low Bake (ULB) Technology for Coatings

The Ultra Low Bake (ULB) technology consists of reducing the curing time or curing temperature of powder coatings. Linked to this reduction in time or temperature (which can reach up to 35%) is the reduction in the amount of gas used in the curing ovens of customers and partners, lowering GHG emissions.

WEG partners who employ such technology in their production line, in addition to reducing environmental impact, have a significant increase in productivity and competitiveness. WEG has forty products developed for this purpose.

Material efficiency and environmental assessment of the product

In its value chain, WEG adopts initiatives in line with the principles of the circular economy, using practices that include the reuse of process residues as raw material, like stamping steel scrap used to make castings, and the adoption of programs to recover materials at the end of the product life cycle through reverse logistics and replacement plans.

The application of these concepts and practices allowed WEG to achieve a material efficiency rate close to 85%. WEG is also constantly improving and evolving the energy efficiency of its products and retrofit solutions to extend the service life of some product lines. Qualified teams work on the processes to develop new products, on the design of new lines and in the implementation of more efficient industrial processes.

WEG applies the LCA (Life Cycle Analysis) to generate the EPD (Environmental Product Declarations) according to the customers’ demands, intending, in the coming years, to expand the application of these tools.

Saiba mais sobre as ações da WEG em Sustentabilidade

WEG Portugal acolhe a primeira edição do Global Summit – Sourcing & Procurement da WEG

WEG Portugal acolhe a primeira edição do Global Summit – Sourcing & Procurement da WEG

Encontro internacional reúne líderes da área de Compras de dez países para fortalecer a colaboração global, alinhar estratégias e impulsionar a inovação nos processos de sourcing

WEG Tintas na Argentina adota energia 100% renovável em parceria com a 360Energy

WEG Tintas na Argentina adota energia 100% renovável em parceria com a 360Energy

Projeto reforça o compromisso da WEG com a descarbonização da indústria e o uso de fontes de energia limpas.

WEG candidata ao Prémio Nacional de Sustentabilidade com projeto que leva energia limpa e desenvolvimento à Amazónia

WEG candidata ao Prémio Nacional de Sustentabilidade com projeto que leva energia limpa e desenvolvimento à Amazónia

O projeto nasceu com um objetivo claro: transformar uma limitação estrutural numa oportunidade de desenvolvimento, inclusão social e maior autonomia para a comunidade local.

WEG torna-se parceira estratégica da UVE para impulsionar a mobilidade elétrica em Portugal

WEG torna-se parceira estratégica da UVE para impulsionar a mobilidade elétrica em Portugal

A parceria com a Associação de Utilizadores de Veículos Elétricos acompanha o investimento da WEG na linha WEMOB (WEG Electric Mobility), a sua gama completa de soluções para o carregamento de veículos elétricos.

WEG oferece soluções de acabamento técnico para ambientes de saúde

WEG oferece soluções de acabamento técnico para ambientes de saúde

Tecnologia em revestimentos em pó combina proteção, segurança operacional e sustentabilidade em aplicações hospitalares

Grupo WEG
  • Avenida Prefeito Waldemar Grubba, 3300 - 89256-900 - Jaraguá do Sul - SC
  • Telefone: +55 47 3276 4000
  • E-mail: esg@weg.net






 

Instagram LinkedIn YouTube

 



 
WEG - Driving Efficiency and Sustainability