• Collection and Irrigation
  • Automation
  • Power Supply
  • Coatings
  • Animal Comfort
  • Services
  1. Home
  2. Farming & Agriculture - Coatings

Coatings that offer full protection.

Since 1983, WEG has invested in the chemistry of colors, producing liquid and powder industrial paints, enameling varnishes and impregnation resins for electric motors, serving different market segments.

The technology used in our products assists greater productivity as it extends the intervals between maintenance, cutting down costs and, consequently, generating savings.

In order to serve a diversified market that demands high resistance to bad weather combined with the great physical and chemical resistance, WEG presents solutions that join resistance and high performance, from the synthetic enamel to the water soluble paints, ensuring the correct product for your application.

WEG is currently the leader on the Brazilian market in powder paints and varnishes, and enameling and impregnation resins, and it is among the main manufacturers of industrial, marine, anti-corrosive, automotive maintenance and refinish paints, offering high technology products that provide productivity gains, resistance and the promotion of WEG brand.

Products



Liquid Paints

Developed with high-technology raw materials, the liquid paints are recommended for industrial, maintenance, marine, automotive refinish, floor, plastic, glass and mirror painting, complying with most national and international quality and resistance standards.

Powder Paints

Developed for application by means of electrostatics painting, WEG powder paints provide smooth and textured finish that can be used in different applications. Available in polyester, epoxy and hybrid, they have state-of-the-art technology and are suitable for the requirements and needs of each customer



POLYESTER POLITHERM LINE

Good adhesion and flexibility, good physical and chemical resistance offering the advantage of great resistance to weathering and yellowing. Recommended for environments exposed to bad weather or unprotected areas.

Tecnologia - Destaques

 

Tintas Nobac®

As tintas líquidas e em pó WEG NOBAC® inibem a proliferação de bactérias, além de oferecer uma superfície uniforme, de alta resistência química e fácil limpeza. Indicadas para todos os segmentos ligados a saúde, as tintas WEG NOBAC® são adequadas para uso em áreas de processamento de alimentos e outros ambientes nos quais a higiene é primordial.

Tinta W-ECO

Para condições específicas de mercado onde se exige tintas isentas de metais pesados, a WEG desenvolveu as tintas W-Eco e W-Eco R. A linha W-Eco atende a norma NBR NM 300-3:2004 no quesito isenção de metais pesados e a W-Eco R atende a diretiva RoHS. Tecnologia disponível em tinta líquida e pó. Indicadas para máquinas e equipamentos.

Tinta W-ZN

Primeira tinta em pó epóxi anticorrosiva do país, a W-Zn é utilizada como primer anticorrosivo, indicado para revestimento de peças metálicas, podendo até substituir a galvanização química e a zincagem em determinadas situações. Um sistema de fosfatização mais tinta em pó convencional apresenta resistência à névoa salina de 500 horas, enquanto o desempenho do primer W-Zn é superior a 2.000 horas.

Veja outros cases

Veja outros cases

Case Cocari Case Armazenagem de Grãos

Saiba mais sobre as novidades da WEG para o Agronegócio

WEG impulsiona autonomia energética no agronegócio com solução BESS integrada à geração solar

WEG impulsiona autonomia energética no agronegócio com solução BESS integrada à geração solar

Sistema de armazenamento de energia em baterias garante continuidade operacional, reduz custos com energia e amplia o aproveitamento da geração fotovoltaica em granja de ovos férteis no Paraná

WEG fortalece sua presença na Turquia com controle inteligente de velocidade de ventiladores para a fabricação de equipamentos agrícolas

WEG fortalece sua presença na Turquia com controle inteligente de velocidade de ventiladores para a fabricação de equipamentos agrícolas

A tecnologia avançada de inversores melhora a eficiência da ventilação, reduz custos operacionais e apoia processos industriais mais inteligentes

WEG e Grupo Ceolin impulsionam a irrigação inteligente com soluções IoT e monitoramento remoto

WEG e Grupo Ceolin impulsionam a irrigação inteligente com soluções IoT e monitoramento remoto

A digitalização das operações agrícolas otimiza o uso da água, amplia a eficiência dos sistemas de bombeamento e garante conformidade com novas exigências ambientais no cultivo de arroz em larga escala

WEG-CESTARI fornece solução completa para potencializar eficiência energética na Yara Brasil Fertilizantes

WEG-CESTARI fornece solução completa para potencializar eficiência energética na Yara Brasil Fertilizantes

Linha de motorredutores WCG20 oferece maior rendimento ao setor de fertilizantes

Equipamentos WEG dobram a potência de usina termoelétrica em empresa alimentícia

Equipamentos WEG dobram a potência de usina termoelétrica em empresa alimentícia

Bem Brasil é a maior produtora de batata do Brasil e tem investido na geração de energia própria

Por que usar motores WEG no agronegócio?

Por que usar motores WEG no agronegócio?

O aumento da necessidade de novas tecnologias no agronegócio, conectando pessoas e o uso de equipamentos de alta confiabilidade, faz toda a diferença na produtividade das fazendas.

TGM recebe Prêmio LIDE Agronegócio 2019

TGM recebe Prêmio LIDE Agronegócio 2019

Empresa foi a vencedora da categoria “Tecnologia em Agronegócio”

WEG fornece motores à prova de explosão para uma das maiores plantas de amônia do mundo

WEG fornece motores à prova de explosão para uma das maiores plantas de amônia do mundo

Projetados e fabricados pela fábrica da WEG em Maia, Portugal, esses motores à prova de explosão irão acionar bombas d’água para alimentação das caldeiras e bombas de processo.

FS Bioenergia é pioneira na produção de etanol de milho no Brasil

FS Bioenergia é pioneira na produção de etanol de milho no Brasil

Usina conta com soluções WEG de alta eficiência

Zest WEG Group helps farmers to reduce their electricity cost

Zest WEG Group helps farmers to reduce their electricity cost

An effective strategy employed by some of South Africa's most successful farms is to replace the older, less efficient motors whenever they fail

Solução WEG com motores Cooling Tower Direct Drive System reduz custos em parque fabril da maior empresa de suco de laranja do mundo

Solução WEG com motores Cooling Tower Direct Drive System reduz custos em parque fabril da maior empresa de suco de laranja do mundo

Sistema modula a velocidade de acordo a demanda da aplicação, promovendo economia de energia e redução no consumo de água.

WEG Improves the Environmental Impact of the La Corona Sugar Mill in Argentina

WEG Manufacturing in San Francisco, Córdoba, recently installed the largest low voltage variable frequency drive (2280A) controlling a WE...

Innovative system for ventilation in silos cuts down energy costs by 80%

Savings results greater than previous averages of similar WEG solutions.

WEG Solution Reduces Operating Costs for Rice Processor

Project lowers electric energy consumption by 70% and reduces equipment wear.

Energy Efficiency at Cargill

WEG provides solutions that assure productivity and energy savings in the food production process from the first stages of the chain.

Gostou da Solução e quer saber como adquirir? Escolha uma das opções abaixo e encontre o produto que você deseja:

Entre em contato com a gente e tire suas dúvidas.

Fale Conosco
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
  • Eficiência Energética
  • Energia