WEG has been awarded a contract by ENGIE Brasil to supply two new generating units that will increase the capacity of the Jaguara Hydroelectric Power Plant, located in Rio Grande, on the border between the states of Minas Gerais and São Paulo, in the municipality of Rifaina (São Paulo, Brazil). The project is aligned with ENGIE's strategy of investing in high-performance assets powered by 100% clean energy and is the result of its successful bid in Brazil's 2026 Capacity Reserve Auction, held in March this year.
The total planned investment of BRL 1.2 billion will increase the plant's installed capacity by 232 MW through the installation of two new generating units in existing shafts, each with an installed capacity of 116 MW. The new turbines are expected to begin commercial operation in 2030.
The Jaguara Hydroelectric Power Plant became part of ENGIE Brasil Energia's portfolio in 2017. The facility currently has an installed capacity of 424 MW and a firm energy capacity of 324 MW average. The concession is valid until June 2048.
Expansion reinforces the strategic role of hydropower generation
The expansion of the Jaguara Hydroelectric Power Plant reinforces the strategic role of hydropower in the energy transition, considering its essential contribution to meeting peak electricity demand while ensuring Brazil's energy security.
"Jaguara is already an important asset in our portfolio, and this expansion strengthens its role in providing operational flexibility, helping increase the reliability of the national power system while maximizing the use of the existing infrastructure, generating efficiency and sustainability gains," says Rogério Suematsu, Plant Manager of the Jaguara Hydroelectric Power Plant.
WEG is a global technology company providing solutions for the energy sector, with expertise in power generation, transmission, distribution, and energy storage projects. Its portfolio includes hydro and steam turbines, generators, transformers, substations, automation systems, and Battery Energy Storage System (BESS) solutions.
"WEG's participation in the expansion of the Jaguara Hydroelectric Power Plant demonstrates our ability to develop and deliver complete solutions for strategic power sector projects. By combining engineering, technology, manufacturing, and specialized services, we help improve the efficiency and reliability of generation assets, supporting our customers in building an increasingly robust and sustainable energy matrix," emphasizes Paulo Leonardo da Silva Sinoti, WEG Energy Solutions and Services Director.
Modernization works
Alongside the expansion project, the Jaguara Hydroelectric Power Plant is undergoing a comprehensive modernization program that began in July 2023. The works involve investments of more than BRL 500 million, of which approximately BRL 150 million has already been invested.
The project aims to extend the plant's service life while improving its reliability and operational efficiency. The modernization includes upgrades to the four existing generating units while maintaining the plant's total installed capacity of 424 MW. Completion of the modernization works is scheduled for 2029.