WEG announced that the company just signed an agreement with FIAT to become the official supplier of charging stations for their new 500e electric vehicle. 

The contract provides for the inclusion of two types of the WEMOB – WEG Electric Mobility new generation in FIAT´s product catalog, as well as the equipment installation service and technical support to customers. 

Specifically designed to meet power, speed, connectivity and safety requirements when charging FIAT's electric vehicles, WEMOB Charging Stations will be offered to FIAT customers in two different types: WALL, designed for homes and condominiums, and PARKING, specially developed for shared use in public and private parking lots. Both stations are suitable for any voltage in Brazil and have all the protections required by national and international standards. With protection against UV rays and resistant to dust and water splash, the equipment can be installed both indoors and outdoors. 

WEG charging stations are designed and manufactured in Brazil, count on a state-of-the-art design and allow internet connection and management platforms to measure and monitor each user´s consumption (service offered via subscription). In addition, they allow access control via proximity cards (RFID tags) or cell phone apps. 

We are taking another significant step in our strategy of offering efficient, sustainable and intelligent solutions for the electric mobility segment. We also want to provide FIAT customers with a unique experience for a quick and safe recharge”, says Manfred Peter Johann, Managing Director of WEG Automation Business Unit. WEG counts on a wide service network in Brazil and will keep the charging stations updated via Over-The-Air (connection through the customer's internet network), as well as providing spare parts replacement across the country.

New FIAT 500e 

Regarded as Fiat's first 100% electric vehicle, the 500e was entirely redesigned in its third generation: developed on the new EV platform, the car is bigger, more connected, with unique equipment for the segment and with new style, offering an outstanding and modern looking. 

For a type in its category, the 500e offers an autonomy of 320 kilometers, easily covering the average daily motion of around 30 kilometers. Tests performed by Fiat at the automotive site of Betim, state of Minas Gerais, indicated that the car can reach 460 km of autonomy driving at ideal conditions. The electric motor delivers 87kW, which is equivalent to 118HP and the torque gets to 220 Nm, reaching 100 km/h in 9 seconds, and with a reaction of 60 km/h to 100 km/h in 4.8 seconds. 

The FIAT 500e will be sold in Brazil by ten dealerships in nine different cities: Porto Alegre (RS), Curitiba (PR), Florianópolis (SC), Campinas (SP), São Paulo (SP), Rio de Janeiro (RJ), Belo Horizonte (MG), Brasília (DF) and Recife (PE). 

 

About WEG Charging Stations 

  • WEMOB Wall at 220V (single-phase and two-phase) with up to 7.4kW, providing an 80% recharge of the batteries in approximately 4 hours. 
  • WEMOB Parking at 380V and 220V (three-phase) up to 11kW, provides an 80% recharge in approximately 2h 40 minutes.