A project delivered by Southeast Power Engineering has seen a mini power station being installed on the River Thames at Romney weir to produce electricity sustainably using environmentally friendly water driven Archimedes screw generators. The completed design features two WEG W22 Premium Efficiency IE3generators being driven by the screws via a gearbox to produce electricity which now powers Windsor Castle.
The scheme is the brainchild of David Dechambeau, Managing Director of Southeast Power Engineering, who has overseen every step of the design and installation process. The power station has now been generating electricity since July 2013 and is in the final stages of completing testing and commissioning.
The power station consists of two Archimedes screws manufactured by Landustrie, each weighing 40 tonnes, connected to the WEG W22 IE3 class premium efficiency generators, which are now delivering 320kW/hr at peak flow, exceeding the original design criteria.
The WEG W22 IE3 generators were designed and manufactured in Portugal at WEG's dedicated European manufacturing site; they are rated at 185kW and produce electricity at 400V, which is then fed via a 500kVA transformer to an underground line that connects to Windsor Castle as well as the National Grid.
The W22 units are specials in that they are generators based on a W22 motor, the reason being that in this application; when the screws need to be re-started, electricity is used to start the screws turning and then as the speed increases, so the motor function is changed over to a generator and the rotation of the screw is maintained by the water which in turn maintains the generator speed to produce the electricity.
Efficiency was a key target for this application as the installation has a fixed ROI period, at 96% efficiency the WEG motor/generators represented one of the best investments Southeast Power could make in the power transmission design to ensure their six year ROI target was met. The installation has a minimum guaranteed design life of 50 years and Southeast Power has a 40 year tenancy of the site, so reliability and longevity were also very important considerations â if the screws stop turning then there is a direct consequence in terms of revenue.
David Dechambeau comments, "In order to make this project sustainable, it was essential that we selected the most efficient equipment for the construction of this power station. The design called for a reliable generator with superior efficiency ratings and on balance the WEG component definitely fitted the criteria and it was straightforward to install."
David Dechambeau adds, "This is a very important project for us, not only because we are supplying the Royal Household, but also as an initial stepping stone for a number of similar projects. It is essential that we install the most efficient and ecologically sound power plant as possible. The work we are completing now will help to deliver future projects using similar technology as demand for sustainable power is understandably going to increase."
W22 sets the benchmark
The W22 motor sets the standard for affordable energy efficiency in the WEG range; while super-high efficiency IE4 motors are available, the IE3 standard offers 96% efficient W22 machines from fractional kW ratings to megawatt powers off-the-shelf. These machines, whether used as motors or adapted to become generators, satisfy an attractive balance between high efficiency, range, availability and value.
When you look at the total cost of ownership (TCO) for one of the machines over its lifetime the cost of acquisition typically represents only 1% of the total cost of ownership of an electric motor. In contrast, the associated energy savings provided by premium efficiency motors far outweigh this additional investment in purchase price, particularly in applications where the process operates on a 24hr basis.
Green power gets Royal approval
The Windsor hydroelectric project represents an investment of over ÂŁ1.7 million coming from a consortium of private funds, but success was not a foregone conclusion as it has taken several years for a scheme to get off the ground after previous attempts failed due to problems with alternative technology and funding.
The royal household has agreed to buy the power generated by the Romney Weir generators, guaranteeing an income for the project. The Queen already has another hydroelectric plant in Balmoral and the Prince of Wales employs solar panels and wood chip boilers on his estate, the Archimedes screws however are the largest project so far and fit-in with a policy by the Royal Household to both cut bills and reduce its carbon footprint.
Estimates are that the hydro-electric generation capacity is equivalent to 1 million lb of coal per year, effectively reducing carbon dioxide emissions by more than 1,000 metric tonnes per year. The ecological side of the project goes further than just sustainable power generation though, with a new 'fish path' being been built alongside the weir to allow fish and eels to migrate up the river for the first time in centuries.