According to Fanie Steyn, Rotating Machines Manager at Zest WEG Group, a MEPS would significantly reduce the peak power demand on the national grid. Importantly, the step could be made at no cost to government and would also bring substantial savings to industry’s electrical energy costs. 

“The MEPS would phase out the least-efficient electric motor classes by setting a minimum standard for the efficiency of motors imported and sold in South Africa,” he says. “The essential challenge now is that about 280,000 electric motors are imported each year, many of which are low efficiency motors rated at IE1 level as standard.”

Steyn highlights the great strides recently achieved in the efficiency of electric motors. Energy savings of between 2.1% and 12.4%, depending on the individual power rating, can be made by converting from a standard efficiency IE1 motor to a premium efficiency IE3 motor. The capital cost differential is slight and is quickly recouped by lower operating costs.

“It is estimated that as much as 45% of all energy produced globally is consumed by electric motors,” he says. “It is therefore easy to see why improving motor efficiencies has a huge impact on national energy consumption.”

It is significant that more than 42 countries already have MEPS in place. These standards apply mostly to three-phase low voltage motors from 0.75 kW to 375 kW capacity. The MEPS is applied at import stage, so the process would be handled in the conventional manner by customs agencies.

“If the 150,000 low voltage motors entering the country each year were IE3 rated instead of IE1, the national grid could be relieved of about 195 million kWh in a single year,” says Steyn. “This means almost three billion kWh over the next five years.”

He adds that this would also mean lower carbon emissions from power stations. South Africa has committed to reduce these emissions by signing the Paris Agreement in 2016.

“Implementing MEPS will have significant benefits for everyone,” Steyn concludes.

The Zest WEG Group, has a strong commitment to contributing to the development of the African region, and has been servicing the continent for more than 37 years.