Back to My Account

WEG
  • English
    • Français
    • Português de Portugal
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
    • BBBEE & CSI
  • Products
  • Solutions
    • WEG efficiency
    • MEPS
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
    • Français
    • Português de Portugal
    • Português do Brasil
    • Español
  1. Home
  2. Technological Innovation

For WEG, technological innovation mainly concerns the development of new technologies, new products, materials, and tests aimed at increasing efficiency, reducing costs, improving quality, and reducing the raw materials used in products. This is how the company becomes more competitive, conquers new markets, remains sustainable, and contributes to the development of the planet.

In 2024, R$ 1.084 billion was invested in Research & Development. Learn more below about how technology is approached within WEG:

TDP (Technological Development Program)

At WEG, all ideas are organized and arranged by means of the WPQP (WEG Program of Quality and Productivity). Within that is the TDP (Technological Development Program), which gathers the innovation projects for new products and processes. Based on the Technological Strategic Planning, the various projects that will become part of the programs are defined.

Investment in Research & Development

Creative people focused on innovation are essential for the evolution of products and processes. Therefore, WEG invests strongly in its Research & Development team, and in an environment oriented to encourage creativity.

Development Flow of WEG Products

From the generation of the idea to the success on the market

TECNOLOGIA MOTORES WEG EVOLUÇÃO

EFICIÊNCIA
DENSIDADE DE POTÊNCIA [kW/kg]
1960
0,13
1980
0,14~88%
1990
0,14~89,5%
2000IE2
0,15~90,2%

W21 AR Plus

2010IE4
0,15~95,1%

W22 Premium

2010IE4
0,30~96%

W22 Permanent Magnet

2013IE4
0,16~95,8%
2014IE5
0,30 (PM)~96,5%

W22 PM Ultra Premium

2019IE6
0,21 (PM)~97,6%

W50 Magnet

2021IE7
0,21~98,08%

Assynchronous Motors

2022IE9
0,21 (PM)~97,5%

Synchronous Motors

2024IE6
0,21 (PM)~97,5%

W23 Sync+

2024IE6
1,55 (PM)~97,5%

W80 AXgen

Maior eficiência

Maior eficiência

Menor consumo de energia

Menor consumo de energia

Coatings technology evolution

80's

CFW-I

Tecnologia AEG

1991

CFW-01

Primeiro inversor com TECNOLOGIA PRÓPRIA

1992

CFW-02

Micro inversor BT full digital totalmente microprocessado

1993

CFW-03

Inversor BT full digital para altas potências (até 150 HP / 132 kW)

1995

CFW-04

Primeiro microinversor BT WEG com IGBTs

1996

CFW-06

Primeira linha de inversor BT WEG com controle vetorial e certificações internacionais CE e UL

1997

CFW-07

Nova geração de microinversor BT

1998

Microline CFW-08

Geração de inversores BT ultra compacto

1999

Início do P&D de inversores MT em cooperação tecnológica com a Univ. Wuppertal – Alemanha

2000

CFW-09

System drive BT WEG controles U/f, VVW e vetorial. Capacidade de paralelismo para altas potências

2001

CFW-08

Inversor BT para aplicações gerais, filtro RFI interno e versão com alto grau de proteção

2004

CFW-10

Nova geração de microinversor BT. Compacto e excelente custo-benefício para aplicações simples

2004

MVW01

Primeiro inversor MT MVW01 - Inversor com braços de potência de média tensão à até 2.500 HP @ 4.160 V

2005

MVW01-C

Versão compacta do inversor MT até 1.000 HP @ 4.160 V

2007

CFW11

Nova geração de inversor BT para sistemas (system drive)

  • Interface gráfica
  • Ampla faixa de potência,
  • Versão modular que permite paralelismo
  • Versão regenerativa
  • Versão com sistema de refrigeração à ar ou água
2013

CFW500

Geração worldclass de inversor BT para aplicações gerais (general purpose)

2014

MVW3000

Inversor MT com IGBTs de baixa tensão ligados em série, mais competitivo para aplicações mais simples até 12.000 HP @ 13.800 V

2016

CFW300

Geração worldclass de microinversor BT (micro drive)

2017

MVW-01WC

Inversor MT com refrigeração a água para o mercado naval e offshore

2022

CFW900

Geração worldclass de inversor BT para sistemas (system drive)

2022

MVW-01EV

Inversor MT resistente a arco elétrico interno para o mercado O&G

2022

ADV200

Linha de inversores BT para sistemas de alta performance (metalurgia, papel & celulose, plástico e elevação de cargas)

2022

ADP200

Linha de inversores BT para aplicação de bombas hidráulicas

2022

ADL500

Linha de inversores BT para elevadores

2022

TPD32

Linha de conversores AC/DC

Learn more about WEG's technological innovations

WEG partners with MIT

WEG partners with MIT

Industrial relationship program seeks to develop technological innovation in partnership with one of the largest technology centers in the world

WEG and Engie Brasil Energia complete installation of the first national wind turbine

WEG and Engie Brasil Energia complete installation of the first national wind turbine

Wind turbine is part of the project for the first National Wind Turbine, which is intended to develop national technology and production chain for the manufacture and installation of large size equipment in the country

Internet of Things: Interconnecting Industries with Improved Efficiency

Internet of Things: Interconnecting Industries with Improved Efficiency

Bringing its concept to the factories, the Industrial Internet of Things (IIoT) leverages technology advantages for higher efficiency on industrial production processes.

WEG receives National Innovation Award in Brazil

WEG receives National Innovation Award in Brazil

WEG was honored with the National Innovation Award offered by the National Confederation of Industry

WEG creates its Open Innovation Center in Jaraguá do Sul – Brazil

WEG creates its Open Innovation Center in Jaraguá do Sul – Brazil

With an ongoing track record of investments in research, development and innovation, WEG took another step to continue its strategy for developing new technologies, inaugurating the WEG IoT Open Innovation Center

WEG takes part of Sirius, one of the first fourth-generation synchrotron light sources of the world

WEG takes part of Sirius, one of the first fourth-generation synchrotron light sources of the world

The new Brazilian Synchrotron Light Source allows researchers to potentially solve the major problems in any area.

WEG Transformers Africa oil lab helps users avoid transformer failure

WEG Transformers Africa oil lab helps users avoid transformer failure

State-of-the-art oil laboratory offers an extensive range of services to transformer owners.

WEG launches Industry 4.0 solution

WEG launches Industry 4.0 solution

WEG Motor Scan monitors motor data, stores in the cloud and provides access to data by App and IoT platform

WEG presents electric motor for buses at FEIMEC

WEG presents electric motor for buses at FEIMEC

Project shows BUS900 electric traction motor in Augmented Reality

New solution from WEG enables periodic monitoring of motors in order to ensure reliability of production

At this year’s Drives and Controls exhibition WEG will showcase a full range of energy efficient motors and drive solutions for a wide variety of industrial applications.

W60 motor line launched with extended power ratings

The W60 motor platform is now available up to frame IEC 1000 (NEMA 1600) and power ratings up to 16,000 kW (21,500 HP).

The list of most innovative companies in Brazil includes WEG

The list of most innovative companies in Brazil includes WEG

Sponsored by Valor Econômico financial newspaper, the prize was awarded to companies considered the most innovative in each of 18 major economic sectors in Brazil and also to the ten leaders in the overall ranking.

WEG releases its 2025 Integrated Annual Report and highlights progress in sustainability

WEG releases its 2025 Integrated Annual Report and highlights progress in sustainability

Results reflect investments in innovation, people development, and consistent progress in ESG initiatives

WEG presents pathways for the energy transition at Hannover Messe 2026, the world’s largest industrial trade fair

WEG presents pathways for the energy transition at Hannover Messe 2026, the world’s largest industrial trade fair

Company showcases an integrated portfolio of solutions in automation, digitalization, energy efficiency and electrification

WEG launches Breesy® varnish for copper wire enameling with a focus on safety and Sustainability

WEG launches Breesy® varnish for copper wire enameling with a focus on safety and Sustainability

A product free of cresylic acid combines high technical performance, improved occupational environment, and reduced environmental impact

WEG Showcases Cutting-Edge Industrial AI Solutions at the Oracle Innovation Center

WEG Showcases Cutting-Edge Industrial AI Solutions at the Oracle Innovation Center

Collaboration reinforces both companies’ commitment to digital transformation, efficiency, and innovation across multiple sectors

WEG Carries Out Advanced Protection Tests Applied to Digital Substations at the Itaipu Technological Park Laboratory

WEG Carries Out Advanced Protection Tests Applied to Digital Substations at the Itaipu Technological Park Laboratory

Real-time tests validate the reliability of WEG solutions for digital substations, ensuring compliance with ONS requirements.

WEG supplies transformers for solar project in Colombia

WEG supplies transformers for solar project in Colombia

The project reinforces the importance of innovation and the development of efficient solutions that will contribute to clean energy generation in Colombia.

WEG Takes First Place in Época Negócios 360° Ranking

WEG Takes First Place in Época Negócios 360° Ranking

First place in the overall ranking is unprecedented in the Yearbook, which has recognized WEG since 2013 as the Best Company in the Mechanics and Metallurgy segment

WEG Delivers Integrated Wound Rotor Motor Package for Shredder Application in Japan

WEG Delivers Integrated Wound Rotor Motor Package for Shredder Application in Japan

Supply strengthens long-term partnership and simplifies commissioning and maintenance for end user operations.

WEG MEXICO, S.A. DE C.V
  • Carretera Jorobas - Tula Km 3.5, Manzana 5, Lote 1, Fraccionamiento Parque Industrial Huehuetoca, Municipio de Huehuetoca - 54680 - CD. de México y Área Metropolitana / Mexico
  • Phone: +52 55 5321 4275 (Ventas Nacionales) / +52 55 5321 4210 (Ventas Internacionales)
  • Email: info-mx@weg.net
  • para centroamerica contacte: rfq-wmx@weg.net