The first 3 HGF 630C motors where recently manufactured by WEGeuro for LMF Austria with final destination Kuwait. This order was won thanks to the cooperation between Watt Drive and WEG Germany and stands out by being the first big order placed by Watt Drive at WEGeuro.

The electrical and mechanical engineering was made at WEG Portugal with the support of WEG Brazil facing the following main challenges:

• 835kW
• 12 Poles
• 3300V
• ExnA Certification
• Ambient temperature up to 55ºC
• Special Thermal protection Space Heaters and electrical protections such as Surge Arresters

We were pleased to know that all the client expectations were exceeded and that he measured vibration levels below 1mm/s with the motor coupled at their compressor on load test.