• News
  • Download Center
  • Product Selection
United States
Change to Another Country
Search


Media Center
Quick access
News
Products & Solutions

» Home » Media Center » News » Products & Solutions » WEG Automated exhaust system allows reduction of CO2 emissions

June 18, 2010 / Products & Solutions

WEG Automated exhaust system allows reduction of CO2 emissions

Automated exhaustion system uses WEG solution to produce 50% energy savings and reduce CO2 emissions by 23 tons

Bag Filter
Enlarge
WEG Automated exhaust system allows reduction of CO2 emissions
MinimizeMaximizeClose
 
Bag Filter

The installation of an automated filtering system at WEG led to a reduction in CO2 emissions of 23.63 tons per year which represents a 53% decrease from previous emission levels and a 50% energy saving on the operation of the automated extraction system.

 
Bag Filter
Bag Filter
Enlarge
WEG Automated exhaust system allows reduction of CO2 emissions
MinimizeMaximizeClose
 
Bag Filter

This solution is part of the company’s policy towards environmental protection and is a very practical and efficient solution for users in the cement, aluminum and steel industry sectors.

 
Bag Filter

Major environmental and financial benefits were achieved by WEG with the implementation of an automated exhaust system in one of its Foundry plants in Brazil.

The solution has resulted in a reduction of CO2 by 23.63 tons per year, which is equivalent to a 53% drop when compared to the original emission amount and represents a 50% energy savings on the exhaust system. It is estimated that five trees are required to absorb each ton of CO2 from the atmosphere. To absorb the amount of CO2 resulted from WEG’s initiative, 118 trees are required in a year.

Applied to any exhaust system using bag filters, this solution is part of the company’s policy towards environmental protection. The same solution is already under study to be implemented also in cement, aluminum and at steel industry customers.

This is what has been done

The exhaust system with bag filter in this Foundry plant works 24 hours a day, 269 days a year. Due to process variations and demand, at least three deburring machines remain out of operation for about 12 hours a day, resulting in unnecessary extraction from such machines.

A combination of two WEG products were applied on this solution: the WMAGNET (permanent magnet) motor for energy saving from the exhaust systems. Design with constant torque along the whole speed range, this motor keeps the exhaust systems within it is operational characteristics. The second product used is the DPFREG20, which is intended for exhaust system control.

In a joint effort with Renner Textil (textile company), the bag filters life time was extended since they are now made of synthetic fibers, hence less subject to damage. This improvement results from pressure and flow setting required by the process, and it minimizes the possibility of occurring defected in these filters and reduces the emission of particles into the atmosphere. The increase of the bag filters life time, the maintenance cost reduction and the significant decrease in energy consumption on this solution are all factors much appreciated by industries due to the current availability and electric energy cost.

 

Print
Recommend this page


Related content
 
Media Center » News » Corporate
Company is first in the electronics sector in Brazil to receive a recommendation for certification of energy efficiency standard

 
Media Center » News » Products & Solutions
WEG high voltage substations and medium and low voltage motors will equip units to be operational in Brazil by 2013

 
Media Center » News » Products & Solutions
WEG supports application of environmentally friendly products with traction systems for Bus Rapid Transit.


 



WEG Easy
News - What's happening at WEG
Newsletter - Have News sent to you by e-Mail