• News
  • Download Center
  • Product Selection
United States
Change to Another Country
Search


Media Center
Quick access
News
Products & Solutions

» Home » Media Center » News » Products & Solutions » Urban transport with electric buses

November 20, 2009 / Products & Solutions

Urban transport with electric buses

WEG supplies the traction motor for the trolleybus, the bus driven by electrical power. The environment and travel comfort are guaranteed in São Paulo, Brazil.

Trolleybus
Enlarge
Urban transport with electric buses
MinimizeMaximizeClose
 
Trolleybus

With a useful life of approximately 25 years, the vehicle has one of its differentials in the inverter & motor assembly, which is more powerful, lighter and more economical.

 
Trolleybus
Motor
Enlarge
Urban transport with electric buses
MinimizeMaximizeClose
 
Motor

WEG has just introduced one more option for a traction motor (three phase, totally closed) with power up to 185kW, extremely light and compact, in a cast water-cooled housing. This represents a reduction of 400 kg, just in motor weight.

 
Motor

Trolleybus

With a useful life of approximately 25 years, the vehicle has one of its differentials in the inverter & motor assembly, which is more powerful, lighter and more economical. The Trolleybus, popularly known as the electric bus, is apparently the same as the others. However, its great difference is in the motor (with inverter) which is driven by electricity, received from an aerial network.

For large cities, where mass transit is indispensable in citizens’ daily life, the Trolleybus represents an excellent solution for energy savings and for improvement of the environment, reducing air pollution, for it does not release the particles that arise from combustion engines. In addition, it also guarantees a more comfortable trip because the vehicle is more silent than conventional buses.

For this type of application, WEG has just introduced one more option for a traction motor (three phase, totally closed) with power up to 185kW, extremely light and compact, in a cast water-cooled housing. This represents a reduction of 400 kg, just in motor weight.

For manufacturers of Trolleybus, partners like Busscar, Tutto, Eletra and Ibrava, WEG has involved and made a great deal of movement of its engineering team, to develop and adjust the products and software for the solution of each client. The powertrain (AC traction motor and microprocessor controlled vector frequency inverter PLC) is the main WEG component in these vehicles.

Hybrid Bus
The traction motor of 185kW and the vector inverter CFW09 of 600A, dedicated to this application, form a robust powertrain, able to make the bus “squeal its tires” on starting out. However, for normal operations, we limit the maximum torque to avoid unnecessary wear. The traction system also has a generator group (alcohol or gas) which feeds a battery bank, responsible for supplying power to the traction system and for the auxiliary services of the bus.

This type of vehicle may be expanded and become biarticulated, with two bellows, in which it is possible to transport up to 300 people, emitting 80% fewer pollutants than conventional systems and consuming 50% less fuel.

Streetcars
Registered as a part of the historical heritage, the Santa Teresa Streetcar (Bonde de Santa Teresa) is a “treasure” of Rio de Janeiro. It is a mistake to think that it is only for tourists, because for the population of the Santa Teresa neighborhood and region, the Streetcar is one of the main means of transportation.

And, for WEG, it is a point of pride to be able to say that it is part of this history, since it is participating in the renovation of the city’s streetcars. The new vehicles are equipped with two special traction Motors of 70kW each, and one traction inverter of 450A.

For those who have not yet had the opportunity to go to Rio de Janeiro, when you go, don’t miss taking a marvelous streetcar ride in Santa Teresa, enjoying the beautiful view from the top of the mountain of the marvelous city.

Print
Recommend this page


Related content
 
Media Center » News » Products & Solutions
WEG supports application of environmentally friendly products with traction systems for Bus Rapid Transit.

 
Media Center » News » Products & Solutions
New Brazilian trolleybuses use WEG electric traction systems

 

 



WEG Easy
News - What's happening at WEG
Newsletter - Have News sent to you by e-Mail