• WEG Easy
  • News
  • Download Center
United Kingdom
Change to Another Country
Search


Media Center
Quick access
News
Products & Solutions

» Home » Media Center » News » Products & Solutions » WEG solutions deliver reduced energy costs at Cargill

March 22, 2010 / Products & Solutions

WEG solutions deliver reduced energy costs at Cargill

WEG solutions ensure productivity and energy saving in the food production process.

Enlarge
WEG solutions deliver reduced energy costs at Cargill
MinimizeMaximizeClose
 

WEG frequency inverters installed on the motors of the boiler at Cargill in Ponta Grossa, state of Paraná.

 
Enlarge
WEG solutions deliver reduced energy costs at Cargill
MinimizeMaximizeClose
 

Motors installed on 60- HP fans.

 
Enlarge
WEG solutions deliver reduced energy costs at Cargill
MinimizeMaximizeClose
 

200 HP motors installed on fans at Cargill

 

One of the largest food producers in Brazil, Cargill, invests in energy efficiency using WEG optimising solutions. At the beginning of the year (2010), the company installed two WEG frequency inverters on the motors of a boiler at a unit in Ponta Grossa, state of Paraná. The unit is part of a soya bean complex which buys, sells and processes soya and other oil seeds. According to Gilmar Weidner, of WEG’s service network, this installation has produced the expected result. “The customer has quickly achieved his goal, which is to reduce energy, whilst maintaining quantity and quality of output.”

Working together with Cargill in 2009, WEG carried out studies to find the best ways to save energy, rationalize operations and update the production complex. Through examinations in place, several improvement opportunities were identified. These included re-powering of the fan motors, the installation of frequency inverters on the motors for the 200-HP and 60-HP fans, and automatisation of the overall system. With the inverters, it was possible to eliminate the mechanical dampers used on the fans, gaining much higher efficiency from their drive motors (see results below). These results will soon be improved further, as two of the motors on the boiler at Cargill in Ponta Grossa are to be replaced with two of WEG’s new W22 Premium efficiency motors.

Energy efficiency results with 60 HP motor:

- Savings of 37 kWh.
- Estimated savings of 144,607 kWh of electricity per year.
- Return of investment: 11 months.
- Energy savings with motor + frequency inverter: US$ 14,512/year.
- Investment with motor + frequency inverter: US$ 12,236

Application engineering results with 200 HP motor:

- Savings of 48 kWh.
- Estimated savings of 509,416 kWh/year.
- Return of investment of repowering the motor to 150 HP, W22: 7 months.
- Energy savings with motor + frequency inverter: US$ 42,5000/year.
- Investment with motor + frequency inverter: US$ 23,360

New Energy Efficiency law

The W22 Premium motors are already in conformity with the new energy efficiency standard, which will take effect as of January of 2010. They assure high efficiency, reliability and very low operation costs. In fact, the cost/benefit relation of the W22 is excellent, especially in terms of energy savings, but also in terms of reduced levels of noise and ease of maintenance.

Print
Recommend this page


Related content
 
Media Center » News » Products & Solutions
WEG serves the global Oil and Gas industry and other hazardous area markets with the widest range of energy saving motors.

 
Media Center » News » Products & Solutions
President of Mexico Inaugurates Cogeneration Plant with WEG Technology

 
Media Center » News » Corporate
WEG increases its shareholding in Voltran, Mexico, and announced the acquisition of control of the Zest Group, in South Africa.


 



WEG Easy
News - What's happening at WEG
Newsletter - Have News sent to you by e-Mail

© 2012 WEG. All rights reserved